Where is the sd card slot located on a C655-S5542?

Reply
Member
Posts: 2

Where is the sd card slot located on a C655-S5542?

Hi

 

Where is the sd card slot located on a C655-S5542? The specifications stated there is one, but I cannot find it :-(

 

Thanks :-)

Posts: 4,899
Topics: 57
Kudos: 1,685
Solutions: 386
Registered: ‎05-03-2009

Re: Where is the sd card slot located on a C655-S5542?

See page 142 of your User's Guide.  While you're there, you might want to read the whole thing.  It has lots of helpful information.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 2

Re: Where is the sd card slot located on a C655-S5542?

Thank you :-)

 

It did not occur to me it would be UNDER the front of the laptop!!