Upgrade video card on Satellite?

Reply
Occasional Builder
Posts: 96

Upgrade video card on Satellite?

Is it possible to upgarde the video card on my laptop?

Toshiba Satellite L755D-S5218
AMD A6-3400M Quad-Core CPU
8 gigs RAM
Windows 7
Posts: 1,735
Topics: 48
Kudos: 885
Solutions: 135
Registered: ‎10-22-2011

Re: Upgrade video card on Satellite?

the video is integrated on the motherboard, there is nothing to upgrade.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD
Member
Posts: 1

Re: Upgrade video card on Satellite?

"The AMD Radeon HD 6520G is an integrated processor graphics card for mid-range laptops"
From here.

 

As your video card is integrated you cannot upgrade it because it is part of your motherboard.

 

The best way to increase performance would be to upgrade to 6 or 8 GB ram as the OS will share it with the video card.

Your system supports up to 8GB ram ddr3 1333:

us.toshiba.com/computers/laptops/satellite/L750/L755D-S5218/

 

A cheap upgrade would be to buy more ram: pc3-10600s.

 

What to do?

1. Check how many sticks of ram you have by using this program:

http://www.cpuid.com/softwares/cpu-z.html

2. If you have 1 x 4GB ddr3 ram then you need to buy 4gb ddr3 1333 ram ( pc3-10600s ), if you want to have 8 GB ram and more shared video ram.

3. If you have 2 x 2GB dd3 ram then you have 2 options: to buy 4 gb ddr3 1333 ( pc3-10600s ) and have 6GB total ram (one from the old sticks would remain on the laptop), or to buy 2 x 4 gb ram ( pc3- 10600s ) and have 8 gb total ram.

 

The "pc3-10600s" stands for ddr3 1333 MHz

If you can find a cheaper pc3-10600, without the "s", buy it as it is the same (some manufacturers have "s" at the end and others don't).

Occasional Builder
Posts: 96

Re: Upgrade video card on Satellite?

OK thanks. I suppose a RAM upgrade would be cheaper than upgrading the entire motherboard.Smiley Happy

Toshiba Satellite L755D-S5218
AMD A6-3400M Quad-Core CPU
8 gigs RAM
Windows 7