Satellite M305D-S4840 sound driver for XP

Reply
Member
Posts: 3
Accepted Solution

Satellite M305D-S4840 sound driver for XP

I have a Toshiba Satellite M305D-S4840 laptop which I have downgraded to Windows XP. Everything works perfect except that I have no sound and cannot locate the drivers. The sound hardware is ATI IXP SB600 High Definition Audio Controller. The Toshiba drivers page has nothing for the sound on the website, can anyone help?
Member
Posts: 3

Re: Satellite M305D-S4840 sound driver for XP

Hi again,

 

Thanks for the assistance... the second driver you gave me also did not work... same error message. However, upon checking again in the device manager, I saw that my sound card hardware had changed from "PCI Device" with a yellow question mark to "High Defintion Audio Bus" or something simular with a red X. I right clicked and enabled it and it went back to a yellow question mark. Then I installed again the first driver you gave me and this time it did not give the error and went into the setup menu and I was able to successfully install the driver. Everything is now working fine and I have audio.

 

Thanks again for the help!

View solution in original post


All Replies
Posts: 46,794
Topics: 83
Kudos: 8,801
Solutions: 3,146
Registered: ‎12-04-2008

Re: Satellite M305D-S4840 sound driver for XP

Try this one...

 

Conexant Audio Driver for Windows XP

driver_audio_conexant_os2008304a.exe

-Jerry
Channel 9
Member
Posts: 3

Re: Satellite M305D-S4840 sound driver for XP

Thanks for the driver link, I downloaded it and ran the file, it unzips and begins the installation and then fails - giving me the error: "Driver Installation Failed: Could not find the MEDIA device for this driver." Every time I boot up the laptop Windows XP sees the "PCI Device" and asks for a driver, allowing Windows to go online and search also turns up nothing - checking in device manager shows that all the audio codecs are installed, just no audio controller.

 

Any thoughts?

 

Thanks! 

Posts: 46,794
Topics: 83
Kudos: 8,801
Solutions: 3,146
Registered: ‎12-04-2008

Re: Satellite M305D-S4840 sound driver for XP

The Vista driver for your Satellite M305D-S4840 works for these computers..

 

Satellite M300-ST4060, M305-S4815, M305-S4819, M305-S4820, M305-S4822, M305-S4826, M305D-S4830, M305D-S4831, M305D-S48331, M305-S4860, M305D-S48441, M305-S4848, M305D-S4844, M305D-S4840, M305-S4835, M305D-S4833, M305D-S4828, M305D-S4829, P300-ST3014, P305D-S8816, P305D-S8818, P305-S8814, P305D-S8819, P305D-S8836, P305D-S8834, P305-S8842, P305-S8838, P305-S8832, P305-S8830, P305D-S8829, P305D-S8828, P305-S8826, P305-S88541, P305-S8854, P305-S8848, P305-S8857, P305D-S8845, P305-S8837, P305-S8844, P305D-S88361, P305-S8825, P305-S8824, P305-S8823, P305-S8822, P305-S8820, U400-ST5404, U405-S2820, U405-S2817, U405-SP2803, U405-S2856, U405D-S2848, U405-S2854, U405D-S2846, U405D-S2852, U405D-S2850, U405-S2833, U405-S2830, U405-S2824, U405-SP2801, U405-ST550W, U405D-S2870, U405-S2882, U405-S2878, U405D-S2874, U405D-S2863, U405-S2857, U405-S2826

 

Satellite Pro M300-EZ1001X, M300-S1002X, M300-EZ1001V, M300-S1002V, U400-S1001X, U400-SP2804C, U400-SP2908C, U400-SP2908R, U400-SP2908A, U400-SP2804R, U400-S1002V, U400-SP1801, U400-SP2804, U400-S1001V

 

Other Models All models having model/part numbers beginning in PSMD4U

 


The XP driver I gave you (driver_audio_conexant_os2008304a.exe) is provided for these machines..

 

Satellite P300-ST3014, P305-S8814, P305-S8820, P305-S8822, P305-S8825, P305-S8826, P305-S8832, P305-S8842, P305-S8837, P305-S8838, P305-S8830, P305-S8824, P305-S8823, U400-ST5404, U405-S2820, U405-S2817, U405-SP2803, U405-SP2801, U405-S2854, U405-S2833, U405-S2830, U405-S2824, U405-S2826

 

Satellite Pro M300-EZ1001X, M300-S1002X, M300-EZ1001V, M300-S1002V, U400-S1001X, U400-S1001V, U400-SP1801, U400-S1002V

 

Other Models All models having model/part numbers beginning in PSMD4U

 


Notice that some machines are on both lists. I can't explain why it didn't install.

 

Here's an earlier version that should work for the same reason...

 

       driver_audio_conexant_27320D.exe

 

-Jerry
Channel 9
Member
Posts: 3

Re: Satellite M305D-S4840 sound driver for XP

Hi again,

 

Thanks for the assistance... the second driver you gave me also did not work... same error message. However, upon checking again in the device manager, I saw that my sound card hardware had changed from "PCI Device" with a yellow question mark to "High Defintion Audio Bus" or something simular with a red X. I right clicked and enabled it and it went back to a yellow question mark. Then I installed again the first driver you gave me and this time it did not give the error and went into the setup menu and I was able to successfully install the driver. Everything is now working fine and I have audio.

 

Thanks again for the help!

Posts: 46,794
Topics: 83
Kudos: 8,801
Solutions: 3,146
Registered: ‎12-04-2008

Re: Satellite M305D-S4840 sound driver for XP


Then I installed again the first driver you gave me and this time it did not give the error and went into the setup menu and I was able to successfully install the driver. Everything is now working fine and I have audio.

 

Thanks again for the help!


 

Happy to hear of your success! Thanks for giving us the details.

-Jerry
Channel 9