Satellite L775-S7130 vs. L775D-S7108

Reply
Highlighted
Occasional Contributor
Posts: 11
Accepted Solution

Satellite L775-S7130 vs. L775D-S7108

Hi,

 

Could someone please tell me if it's worth 100.00 to purchase the S7130 over the S7108?

 

I purchased the S7108 a couple of days ago, but I can return within 30 days.

 

I see now where the S7130 is on sale and I can pay 100.00 more for that model. Would the upgrades be worth the extra 100.00?

 

Would it be faster, have better resolution, better speakers, etc.?

 

Thanks.


Accepted Solutions
Occasional Contributor
Posts: 11

Re: Satellite L775-S7130 vs.

Thanks again Jerry.  No, that doesn't make a bit of difference. I'll never fill up more space if I had it. I think I'll keep my computer and save the 100.00.

View solution in original post


All Replies
Posts: 47,680
Topics: 85
Kudos: 9,089
Solutions: 3,214
Registered: ‎12-04-2008

Re: Satellite L775-S7130 vs.

Satellite L775-S7130 (PSK3SU-07W020)

 

Satellite L775D-S7108 (PSK40U-07N00R)

 

Compare the specs above.

 

I expect the resolution and sound are the same.

 

Maybe these help.

 

   AMD Quad-Core A6-3420M vs Intel Core i3-2350M processor

 

   AMD Radeon HD 6520G vs Intel HD Graphics 3000

-Jerry
Channel 9
Occasional Contributor
Posts: 11

Re: Satellite L775-S7130 vs.

Thanks Jerry. I had looked up each computer's specs but I'm not computer suavy so not sure what some of the specs meant as far as how they make the computer perform. These terms don't mean too much to me.

 

When looking at the sites you listed, I guess I it says maybe not worth 100.00 to upgrade? and maybe the computer that I bought will perform just about as well as the S7130?

 

What I take from the links is that I have a better graphics specs but the i3 will run faster. When we say 'fun faster', is there that much noticable difference?

 

Thanks so much for you reply.

Posts: 47,680
Topics: 85
Kudos: 9,089
Solutions: 3,214
Registered: ‎12-04-2008

Re: Satellite L775-S7130 vs.

I would classify them as having essentially the same performance.

 

The main difference in my book is 140 GB in the hard drive capacity, if that matters.

-Jerry
Channel 9
Occasional Contributor
Posts: 11

Re: Satellite L775-S7130 vs.

Thanks again Jerry.  No, that doesn't make a bit of difference. I'll never fill up more space if I had it. I think I'll keep my computer and save the 100.00.

Posts: 47,680
Topics: 85
Kudos: 9,089
Solutions: 3,214
Registered: ‎12-04-2008

Re: Satellite L775-S7130 vs.

I would too. (Some would not consider it an upgrade.)

-Jerry
Channel 9