Satellite L305-S5968 Vista Recovery Disk Download?

Reply
Member
Posts: 1

Satellite L305-S5968 Vista Recovery Disk Download?

My computer took a shock due to lightning. I have identified the hard drive as having been bad. The BIOS doesn't even recognize it and I am unable to recover anything off of it. I had another hard drive lying around that had a Linux OS installed on it, so I installed it and whala, my computer works great. The only problem, I need Windows for work.

 

Is there a place where I can download an .iso for the recovery disk? Or, do I have to order one?

 

Download would be much easier.

 

Thanks

Posts: 47,991
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: Satellite L305-S5968 Vista Recovery Disk Download?

[ Edited ]

 

Satellite L305-S5968 

 


Download would be much easier.


So everybody says. But Toshiba offers only this.

 

   Order Toshiba Recovery Media

-Jerry
Channel 9