Motherboard swap

Reply
Member
Posts: 1

Motherboard swap

I have a Toshiba Satellite L305D-S5934 PSLC8U-03701Q AMD Turion X2 Dual-core mobile processor RM-70 with a failed motherboard. The MB specs are: 

Pn# 1310A2175011      BD system

SPS# V000138200

IEC s/n X092M80LMWS

Date code; J9024  Rev: 5.00

Lan Mac: 001E339D5D52

I want to replace it with a motherboard from another (same)L305D-S5934. The specs on this motherboard are:

Pn# 1310A2175011      BD system

SPS# V000138200

IEC s/n X092M82D4A2

Date Code; J9024  Rev:2.00

Lan Mac: 001E33A18875     

Question: Are these 2 motherboards compatible, if not is there anything I can do? Thanks

Posts: 1,735
Topics: 48
Kudos: 889
Solutions: 135
Registered: ‎10-22-2011

Re: Motherboard swap

yes, you should be able to swap them with no issues.

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD