I need help flashing bios with usb flash drive

Reply
Member
Posts: 2

I need help flashing bios with usb flash drive

Hello, I'm trying to flash my Bios with a usb flash drive. My laptop is a Toshiba Satellite L305D-S5928

I know how to boot from the usb but I do not know to make the flash stick a bootable drive. All i could find for flashing my bios is an iso. and i dont have a disk to burn it to so usb is my only option. My bios has a virus and will not let me instal windows. Im hoping that it will let me flash so i dont have to replace it. Can some one please tell me how and what drivers i need to usb flash my bios ?

Super Advisor
Posts: 1,472

Re: I need help flashing bios with usb flash drive

[ Edited ]

The instructions here are for a botched bios recovery, but it explains how to make a USB flash drive bootable and has the links to files that will make it easier to do.

http://forums.mydigitallife.info/threads/2105-BIOS-Recovery-procedures?p=26249#post26249

Welcome to the Toshiba user forums.
For those of you who do not know what a user forum is, it is a community of users who volunteer time to help other users. Anyone can participate. It's 100% voluntary.
Being super active is never a requirement
Member
Posts: 1

Re: I need help flashing bios with usb flash drive

 

For the other people that will end up here. This blog post shows a good way to make a bios update using an usb disk.

http://benobs.blogspot.com.br/2012/04/toshiba-z835-p330-bios-update-from.html