How to get in to BIOS? Satellite P875-S7200

Reply
Member
Posts: 1

How to get in to BIOS? Satellite P875-S7200

[ Edited ]

This thing is a joke... all I want to do it boot off the CD but I cant even get access to BIOS.... Hold esc, f2, f12, delete... nothing works.  Oh and on a sidenote how do I install the graphics drivers? I keep getting code 12 not enough available resources.  Most annoying laptop I have ever worked on......

 

 

 

EDIT: You have to HOLD F2 BEFORE you turn on the computer, thats a little excesive IMO with no clear instructions on it.

 

Still have the video issue... Code 12... Intel HD Graphics 4000

Posts: 1,735
Topics: 48
Kudos: 888
Solutions: 135
Registered: ‎10-22-2011

Re: How to get in to BIOS? Satellite P875-S7200

There are plenty of posts on here telling people how to access the BIOS with fast boot enabled.  As well, Toshiba has a utility that you can use to set the boot priority in windows.  Your driver is on Page 2 of the drivers on the support page for your model:

 

http://www.csd.toshiba.com/cgi-bin/tais/support/jsp/modelContent.jsp?ct=SB&os=&category=&moid=338554...

______________________________________________________
Qosmio X875 i7-3630QM, 32GB RAM, OCZ SSD Qosmio X505 i7-920XM, PM55, 16GB RAM, OCZ SSD
Satellite Pro L350 T9900, GM45, 8GB RAM , Intel 320 SSD (my baby) Satellite L655 i7-620M, HM55, 8GB RAM, Intel 710 SSD
Member
Posts: 8

Re: How to get in to BIOS? Satellite P875-S7200

[ Edited ]

Still have the video issue... Code 12... Intel HD Graphics 4000




Reinstall your OS -> Install The Chipset software first, then the display driver -> Install another driver.

 

That should resolve your problem.