Headphone jack doesn't work

Reply
Member
Posts: 2

Headphone jack doesn't work

Hello,

 

I have a Satellite  P205-S6307 using VistaI recently tried to use my headphone jack to listen to a video, but I get no soundWhen I plug in the headphones, I don't even get staticThese headphones do not have a volume switchHowever, they work fine on other computersAlso, when I do plug them in, the computer speakers still play and don't shut offI've checked all the settings that I can find that relate to audio speakers-headphones etc. but nothing works.  

 

I'd appreciate any suggestions.

 

Thanks

 

 

ST 

YSL
Member
Posts: 1

Re: Headphone jack doesn't work

Try this: Make sure your headphones are hooked up. Go to the Start button, click Control Panel, click Sound, Click Headphones, click Set as Default. Hope it works for you!
Member
Posts: 2

Re: Headphone jack doesn't work

Hello,

 

Thanks for the reply.  Yes it did work! But only briefly. If I unplugged the headphones and then replugged them in they wouldn't work and neither would the laptop speakers.  Then I could reset he default and the laptop speakers would work again.  

 

I at least got it to work some. That's more than I've ever been able to do.

 

Thank you again,

 

 

ST 

Regular Advisor
Posts: 233

Re: Headphone jack doesn't work

Nice to see you up and running now !

 

 

 

 Cheers !

________________________________________________________________________
"I'm Not the Message... Just the Messenger.. i Don't Play the Music... The music plays through me... Im just a Channel..... That's all I AM "