HELP!!! VOLUME KEYS AND SOUND KEY NOT WORKING PROPERLY

Reply
Member
Posts: 2
Accepted Solution

HELP!!! VOLUME KEYS AND SOUND KEY NOT WORKING PROPERLY

[ Edited ]

Hi guys, Heeeeeeelp!

 

I just bought Toshiba Satellite C850-190.

Operating system - W7 Ultimate already installed, all other programs I need also installed. But I have a problem with the volume and sound keyes on the keyboard.

I opened a movie with the KM player and I wanted to increase / decrease the volume. That didnt happen, but the window with the movie was closed, only the picture, the sound was OK.

The sound button also has a problem. It minimize / maximize the window. 

My question is is this from a missing driver? If yes, where I can find keyboard drivers for my notebook?

How I can solve the problem?

 

Please help me!

Posts: 45,932
Topics: 81
Kudos: 8,227
Solutions: 3,088
Registered: ‎12-04-2008

Re: HELP!!! VOLUME KEYS AND SOUND KEY NOT WORKING PROPERLY

 

Satellite C850-190 (PSKCAE-04Y00LB3) <- somewhere in the Middle East?

 

Satellite C850-190 (PSKCAE-04Y00LB3) <- Bulgaria?

 

In any case, you can look up your drivers here.

 

 

Keyboard drivers are native to Windows. But the function keys are mostly controlled by this utility.

 

   Toshiba Value Added Package for Windows 7 - 64 Bit, 1.6.0021.640203, 28/12/12

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 45,932
Topics: 81
Kudos: 8,227
Solutions: 3,088
Registered: ‎12-04-2008

Re: HELP!!! VOLUME KEYS AND SOUND KEY NOT WORKING PROPERLY

 

Satellite C850-190 (PSKCAE-04Y00LB3) <- somewhere in the Middle East?

 

Satellite C850-190 (PSKCAE-04Y00LB3) <- Bulgaria?

 

In any case, you can look up your drivers here.

 

 

Keyboard drivers are native to Windows. But the function keys are mostly controlled by this utility.

 

   Toshiba Value Added Package for Windows 7 - 64 Bit, 1.6.0021.640203, 28/12/12

-Jerry
Channel 9
Member
Posts: 2

Re: HELP!!! VOLUME KEYS AND SOUND KEY NOT WORKING PROPERLY

Hi Jerry,

 

Yes, exactly, Bulgaria.

Thanks for your help. Now everythig is OK. Everything is working perfectly when I isntalled the correct drivers.

 

You are great! Smiley Happy 

 

 

Zori