Enter L655D Bios after Fast Boot

Reply
Member
Posts: 7
Accepted Solution

Enter L655D Bios after Fast Boot

So i enabled Fast boot .. nice feature ,, PC boots Quicker Smiley Tongue ,,, But now i can't seem to Enter the Bios ,,,, Any Clues as to how it's done now that fast boot is enabled ? Smiley Surprised


Accepted Solutions
Member
Posts: 7

Re: Enter L655D Bios after Fast Boot

OK, found the Fix in the Manual .. lol ...

 

Click Start, All Programs, TOSHIBA, Utilities, and then HWSetup ..

 

Kinda Kool That i can adjust Bios Settings from within Windows Smiley Wink

View solution in original post


All Replies
Member
Posts: 7

Re: Enter L655D Bios after Fast Boot

OK, found the Fix in the Manual .. lol ...

 

Click Start, All Programs, TOSHIBA, Utilities, and then HWSetup ..

 

Kinda Kool That i can adjust Bios Settings from within Windows Smiley Wink

Regular Contributor
Posts: 217

Re: Enter L655D Bios after Fast Boot

You can also hold down the ESC key and then power on. 

 

It should take you to the BIOS Setup.  This is what you do if you hard disk crashed. 

 

 

Member
Posts: 7

Re: Enter L655D Bios after Fast Boot

Tried that.... didnt work

Regular Contributor
Posts: 217

Re: Enter L655D Bios after Fast Boot

I am so sorry, it is the F2 key. 

 

Hold down the F2 key and then power on.  I just tried it and it worked.

 

Again, I am sorry for the miss information.

Member
Posts: 7

Re: Enter L655D Bios after Fast Boot

[ Edited ]

OK kool, that worked.... Ok problem is when i use fast boot the internal mic is disabled for some strange reason ...

Regular Contributor
Posts: 217

Re: Enter L655D Bios after Fast Boot

Let me try that on my machine.  I will get back to you. 

 

 

Regular Contributor
Posts: 217

Re: Enter L655D Bios after Fast Boot

I just tried that. 

 

Sure enough the mic is out.  This only happens when in Fast Boot.  I spoke to Support, I got through, they are investigating it.  If I find a solution I will post it here. 

 

Good luck,

Member
Posts: 7

Re: Enter L655D Bios after Fast Boot

Kool thanks ... hope they release a patch/fix soon ...

Member
Posts: 7

Re: Enter L655D Bios after Fast Boot

Just a note that I just did a Bios Update and the Microphone issue is Fixed..

The mic now works even when fast boot is enabled.. Smiley Happy

Member
Posts: 1

Re: Enter L655D Bios after Fast Boot

Pres and hold F12 and power button until display boot menu. now select setup.