DVD Drive not recognized

Reply
Member
Posts: 8

DVD Drive not recognized

My DVD drive is not recognized. When I load a CD or DVD, I get nothing. When I navigate to the drive using Explorer, the resulting dialog says, "Please insert disc" or something similar.

 

When I use the Diagnostic tool, and check only the drive for analysis, and run the diagnostics, the result that comes up is "SKIP".

 

The laptop is relatively new, and I have disabled a handful of the plethora of Toshiba "crapware" services and startup programs, so I probably disabled some important service. But I can't figure out which. Any ideas?

 

Thanks a bunch.

Posts: 46,771
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: DVD Drive not recognized

I infer from your other message, you have Windows 7. Please give what you know about the model when you post here.

 

Open Device Manager (devmgmt.msc), expand DVD/CD-ROM drives, and double-click the drive. What does Device status have?

 

  

-Jerry
Channel 9
Member
Posts: 8

Re: DVD Drive not recognized

[PC Information]
 Model Name     Satellite P770
 Part Number    PSBY3U-0NQ03J
 Serial Number  XB245941K
 OS Version     Microsoft Windows 7 Professional    6.1.7601   Service Pack 1
 BIOS Version   1.60
 CPU            Intel(R) Core(TM) i7-2670QM CPU @ 2.20GHz
 Physical Memory6144MB RAM
 Hard Disk Capacity482,350,198,784 [Byte]   449.224 [GB]
 Hard Disk Free Space Capacity405,263,417,344 [Byte]   377.431 [GB]
 Video          NVIDIA GeForce GT 540M    version=8.17.12.6885
 Screen Resolution1600 x 900 Pixels
 Color Quality  True Color (32 Bit)
 Sound          Realtek High Definition Audio   version=6.0.1.6323
                Intel(R) Display Audio   version=6.14.0.3074
 Network        Realtek PCIe GBE Family Controller   version=7.46.610.2011   MAC Address=B8:70:F4Smiley Very Happy8:4E:66
                Realtek RTL8188CE Wireless LAN 802.11n PCI-E NIC   version=1005.12.105.2011   MAC Address=74:31:70:49:27:45
 Modem          None
 Internet Explorer9.0.8112.16421
 IDE Device     Hitachi HTS547550A9E384
                TSSTcorp CDDVDW TS-L633F   FW version=TF01

 

Dev Manager status:  "This device is working properly."

 

I just tried again, inserting a music CD into the drive. When I tried to exand the drive and see the contents, the drive door popped open and the dialog box came up, "Insert a disc. Please insert a disc into drive D:'.

Posts: 46,771
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: DVD Drive not recognized

 

Satellite P770 (PSBY3U-0NQ03J)

Windows 7 Professional   

 

Please give us that and the bitness of Windows (64-bit?) when you post.

 

 

Try this. In Device Manager, right click the drive (the device you double-clicked) and click Uninstall. Then click Scan for hardware changes on the Action menu and reboot.

-Jerry
Channel 9
Member
Posts: 8

Re: DVD Drive not recognized

I would say that's "none of your bit-ness" but that might be impolite.

 

It's Windows 7 Pro, SP1

Intel Core i7-2670QM processor

64-bit

 

By the way, no success with uninstalling the drive from the device manager. I could right click and uninstall, and the drive (and category) would disappear. After I restarted the computer, the drive would show up -- already installed, without any "found new hardware" wizard running, at least none that I saw -- and the behavior would be the same.

 

Great idea, I should have thought of it...but it did not work. I really appreciate your help. I've attached a screen shot of some possibly relevant shizzle.

 

By the way, I do not think I have used this drive even once since I got the computer. No need for it yet. So it's possible the drive or driver was DOA and I never noticed until now.

 

 

 


Posts: 46,771
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: DVD Drive not recognized

Sorry, I don't have any other suggestions. I'm a Windows specialist. So far as I know the drive is dead.

-Jerry
Channel 9
Member
Posts: 8

Re: DVD Drive not recognized

You're a gentleman and a scholar. Thanks for your help, and timeless effort helping others on this site.

Posts: 46,771
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: DVD Drive not recognized

Thank you for the kind words.

-Jerry
Channel 9
Member
Posts: 3

Re: DVD Drive not recognized

[ Edited ]

Here's the answer - It's not a driver problem actually.

Just ran into this helping a client that I recently set up with a new Toshiba Satellite L755.

Suddenly the CD / DVD drive stopped working.  Just like many posts on the forums - it didn't show up in Computer at all.

A quick registry tweak will do the trick.  The Microsoft Fix-it didn't work for me - it returned an error.  I followed the manual removal instructions, and it worked like a charm.

http://support.microsoft.com/kb/314060

 

Happy Computing

www.mytechbutler.com