C655 Laptop how do I start web cam?

Reply
Member
Posts: 1

C655 Laptop how do I start web cam?

 
Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: C655 Laptop how do I start web cam?

C655 Models number well into the hundreds so give your COMPLETE model info as in my example below if you have to post back.  Meanwhile, Go to Start/All Programs/ Toshiba/Utilities/Web Camera Application.  Some models, when you get to Toshiba, click on Media and Entertainment and then click on Web Camera Application. I'm sure your User's Guide tells you how but I can't even use that reference since I don't have your full model number.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit