Boot problems

Reply
Member
Posts: 1

Boot problems

[ Edited ]

Satellite L450D

- AMD Turion X2 Dual-Core Processor RM-74
- 4096 MB (2048 +2048) DDR RAM (800MHZ)

Windows® 7 Home Premium 64-bit
when I power on laptop it hangs on Toshiba startup screen 

I press F2 it says loading but hangs and powers off after 2-3 mins

press F12 does exactly the same as F2 any solutions please

 

Regular Contributor
Posts: 112

Re: Boot problems

If you can't get into the BIOS (using F2) without the system hanging (freezing up) the motherboard is probably bad.  Check in your area to see if any technicians offer repair estimates for free.  Maybe they will give you a better idea what is wrong.  Due to the high labor costs, most techs charge, repairing this type of problem would probably be more expensive then getting a new computer.  An alternative to repair would be to sell it (as is) on ebay and use that money towards a new system.  The toshiba sales on ebay are very active and you can usually get close to $100. even in "non-working" condition.

 

Enjoy,

Mike