Wireless adapter not working...

Reply
Member
Posts: 2

Wireless adapter not working...

Hi,

I have a Toshiba satellite l25-s1216 I have downloaded the drivers for the LAN and wireless.Now I can connect to the internet via Ethernet, but can not do so via wireless, error is adapter not installed when it is. I have check device manager and it is there but not being seen. It also says that there is no matching driver when I install the driver.

Posts: 47,509
Topics: 84
Kudos: 9,030
Solutions: 3,199
Registered: ‎12-04-2008

Re: Wireless adapter not working...

 

Satellite L25-S1216 

 


I have check device manager and it is there but not being seen. It also says that there is no matching driver when I install the driver.

Please quote what Device Manager has for Device status. Put it on a line all by itself.

 

Is this what you used for the driver? Quote that message separately too.

 

   Atheros Mini PCI Wireless Lan (802.11 a+g/g) Driver for Windows XP/2000

-Jerry
Channel 9
Member
Posts: 2

Re: Wireless adapter not working...

Well the driver is showing up in the device manager, and yes that is the driver that I downloaded that is in your reply.

Posts: 47,509
Topics: 84
Kudos: 9,030
Solutions: 3,199
Registered: ‎12-04-2008

Re: Wireless adapter not working...

I would like exact quotes of the messages.

 

(1) The one in Device Manager (the "Device status").

 

(2) And the one that occurs when you attempt to install the driver.

 

Please don't bury those message. Put each on a separate text line.

 

(Microsoft messages rarely mean what they say.)

-Jerry
Channel 9