Wireless adapter auto switch-off - Toshiba Satellite P755-S5215

Reply
Member
Posts: 2
Accepted Solution

Wireless adapter auto switch-off - Toshiba Satellite P755-S5215

I'm faced with a weird issue with my 10-month old Toshiba Satellite P755-S5215 running Windows 7. Whenever the laptop is running on battery (i.e. without AC support) the wireless adapter keeps turning itself off, and the active connection is imediately terminated. Pressing the wireless button does not work; I need to repair it using the network diagnostic utility. The connectivity comes back for a few seconds before history repeats itelf. The reason I'm suspecting this to be a software issue is that the problem never arises when the laptop is plugged into a wall socket. Has anybody else faced a similar issue? Kindly advice.

Posts: 45,953
Topics: 81
Kudos: 8,252
Solutions: 3,088
Registered: ‎12-04-2008

Re: Wireless adapter auto switch-off - Toshiba Satellite P755-S5215

 

Satellite A505-S6981

 

 

If CB's suggestion doesn't take care of the problem, see Microsoft's KB928152.

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 4,812
Topics: 56
Kudos: 1,536
Solutions: 370
Registered: ‎05-03-2009

Re: Wireless adapter auto switch-off - Toshiba Satellite P755-S5215

Type Dev in Start/Search box and click on Device Manager. Double click Network Adapters and double click the Wireless LAN Adapter. Click on the Power Management tab and uncheck the box that says "Allow the computer to turn off this device to save power".

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 45,953
Topics: 81
Kudos: 8,252
Solutions: 3,088
Registered: ‎12-04-2008

Re: Wireless adapter auto switch-off - Toshiba Satellite P755-S5215

 

Satellite A505-S6981

 

 

If CB's suggestion doesn't take care of the problem, see Microsoft's KB928152.

-Jerry
Channel 9
Member
Posts: 2

Re: Wireless adapter auto switch-off - Toshiba Satellite P755-S5215

Thanks CB and Jerry. It was indeed a software issue, and it was resolved on adjusting my power plan to allow for maximum wireless performance.