WIFI ISSUES WITH L635-S3030

Reply
Member
Posts: 1

WIFI ISSUES WITH L635-S3030

[ Edited ]

Anybody having trouble with wifi connection on a satellite l635 -s303.  I am using a Netgear Access Point for connection. Its a model WN802tv2 with the latest firmware.  The laptop connects for about 20 seconds and then re-connects.  I have update firmware for wifi card in laptop.  I have changed security in the access point.  I do a constant ping test to the default gateway and get a general failure after about 20 to 25 packets.  Then it reconnects.  I have two HP laptops and an HP wifi printer. All with no connection problems. I am using WEP for security.

 

Any help would be great.

 

P.S. The Geek Squad at Best Buy  says there is no problems.  I bought this laptop for Christmas. So its about 6 weeks old.

Member
Posts: 6

Re: WIFI ISSUES WITH L635-S3030

If you have a Realtek wireless adapter try downloading the latest version of it from realtek.com.  It works dine on mine.

Occasional Contributor
Posts: 15

Re: WIFI ISSUES WITH L635-S3030

2nd that go to realtek site , fixed the same issue on my wireless netgear setup.