Toshiba Satellite L645 Button Support is not working

Reply
Member
Posts: 1

Toshiba Satellite L645 Button Support is not working

Dear all,

I use Toshiba Satellite L645 Laptop, using windows 7 32 bit.. Suddenly my Button support is not working, there is no animated button on the top of the monitor when i press Fn key, but i still can mute my laptop pressing Fn+ esc, but there's no animated button. how can i fix this problem?

i tried to install the toshiba value added package but the problem is still exist.

can anyone help me fix this problem?

Posts: 47,009
Topics: 83
Kudos: 8,911
Solutions: 3,164
Registered: ‎12-04-2008

Re: Toshiba Satellite L645 Button Support is not working

Try this.

 

   Start > All Programs > Toshiba > Utilities > Settings for Flash Cards

 

Always tell us which Satellite L645 you have. There is a label on the bottom.

-Jerry
Channel 9
Occasional Contributor
Posts: 20

Re: Toshiba Satellite L645 Button Support is not working

i have same problem, my toshiba is L645, windows 7 home premium, corei3.

i've tried your solution so after "Settings for Flash Card", what must i do?

 

thank's before mr. jerry..

Occasional Contributor
Posts: 20

Re: Toshiba Satellite L645 Button Support is not working

i have the solution. in this link http://forums.toshiba.com/t5/Networking-Wi-Fi/Can-t-turn-on-wireless-capability/m-p/190572#M10701

maybe you can check it..

thank's..