Tobisha Wifi Drivers

Reply
Member
Posts: 2

Tobisha Wifi Drivers

Ok Computer crashed and i happened to have an instalation disk of windows vista home basic. All went well until i tried to find drivers, found drivers for everything including the ethernet port and so on, The problem comes form trying to find the driver for the WIFI adapter Ive tried the Toshiba site, and all it gave me was crap, sorry toshiba but you kindaare letting me down. The driver came in a self installing utility which dosent help at all. Tried Driver Genious pro, still dosent work. the WiFi radio glows orange when i turn the swich on (im sure its supposed to be blue) and the Keyboard funtion keys dont work.at all

 

Toshiba SatlliteL305-S5955

Windows Home Basic x32

2 Gig RAM

SATA Hardrive

 

WiFi sticker:

FCC ID: TX2-RTL-RTL8187B

Contains radio device:RT8187B

 

Ive loked on realtek website also same usles compilation of coding downloaded about 200 times so far, i know its a bit too much but can i please have a link to the acctual Working Wifi Driver or instructions on how to use it properly

 

Posts: 47,962
Topics: 85
Kudos: 9,136
Solutions: 3,232
Registered: ‎12-04-2008

Re: Tobisha Wifi Drivers

 

Satellite L305-S5955 

 

This is the correct driver.

 

   Realtek Wireless LAN Driver for Windows Vista (32/64bit) / XP

 

My guess is that you installed things in the wrong order. You should install the Intel chipset software followed by the Intel display driver prior to any other drivers.

-Jerry
Channel 9
Member
Posts: 2

Re: Tobisha Wifi Drivers

Thanks allot ima going to try it now if it works Thank you so much, and if it dosent oh well but still thank you for your time.

Member
Posts: 1

Re: Tobisha Wifi Drivers

Realtek Wireless LAN Driver for Windows 7 (32/64) does´t work under u505-sp2916r, only bluetooth work with switch belong to wireless adapter.

 

El driver no funciona en una satellite u505-sp2916r, en su lugar me aparece el bluetooth que si apago el switch del wifi se apaga el bluetooth

 

Thanks

 

Gracias