TOSHIBA Satellite A665 S6050 wireless connection problems

Reply
Member
Posts: 2

TOSHIBA Satellite A665 S6050 wireless connection problems

This has happened multiple times with my laptop and usually it is fixed with a reboot but this time it's not the same story.

I am not able to connect to any wifi right now because it say my radio hardware switch is turned off. I try using the function keys and I also try to use the little button above the keyboard and this doesn't do anything. My friend said it is possible that the BIOS is doing something wrong. I would like help in any ways possible. Maybe I just have to update my driver? I haven't updated it since I bought the laptop but I never thought to since it didn't prompt me to and since I never had the problem get this serious before. I am running windows 7 64 bit.

Please any help or advice that u guys could give will be greatly appreciated.

Posts: 21,713
Topics: 70
Kudos: 831
Solutions: 482
Registered: ‎10-04-2011

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

Satellite A665-S6050

 

Open Device Manager (search for it in the Start Menu if you need), expand "Network adapters," and tell me what's listed. Is there a yellow exclamation mark next to any of them?

- Peter
Member
Posts: 2

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

very sorry about the late response. i do not have my laptop with me. and i dont remember what the drivers were exactly.

i do remember there being no exclamation signs and all the same drivers that were there when i got it are still there.

lemme get back with u about the specific drivers though if u would like

Posts: 21,713
Topics: 70
Kudos: 831
Solutions: 482
Registered: ‎10-04-2011

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

Yes, let me know just to be sure. Then we'll try reinstalling the drivers.

 

Have you ever needed to make any BIOS changes? If there's nothing you've specifically changed, we can try restoring the BIOS to default settings.

- Peter
Member
Posts: 4

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

I have the same computer and I'm having the same problem.  I checked my device manager and it says that my network adapters are working fine and there are no exclamation marks next to anything.  I don't think I've made any BIOS changes.

Posts: 21,713
Topics: 70
Kudos: 831
Solutions: 482
Registered: ‎10-04-2011

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

Le-Le,

 

What are the names of the network adapters listed in Device Manager?

- Peter
Member
Posts: 4

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

Intel(R) Centrino(R) Advanced-N6200 AGN

Microsoft Virtual WiFi Miniport Adapter

Microsoft Virtual WiFi Miniport Adapter #2

Realtek PCIe FE Family Controllers

 

 

Posts: 21,713
Topics: 70
Kudos: 831
Solutions: 482
Registered: ‎10-04-2011

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

Member
Posts: 4

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

That didn't work.

Member
Posts: 3

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

switch the network card and it will works

Member
Posts: 1

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

I have the same problem and same network adapters as Le-Le.    It's definitely my laptop as an older Dell connects with no issues and my iPhone also connects and stays connected just fine.  I have tried other fixes mentioned on site - changing power management settings, tried to update drivers.  I even tried removing the battery.  No luck.  Everything was working fine until today. 

Member
Posts: 4

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

what do you mean switch network cards?

Posts: 21,713
Topics: 70
Kudos: 831
Solutions: 482
Registered: ‎10-04-2011

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

You might want to try contacting technical support at (800) 457-7777.

- Peter
Member
Posts: 2

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

I have a problem with my satellite, and I went to the Devices, and all of my network adapters are yellow, except the only ones on there are 

-Network Controller (flag)

-PCI Simple Communications Controller (Flag)

-Unknown Device (Flag)

 

Regular Contributor
Posts: 80

Re: TOSHIBA Satellite A665 S6050 wireless connection problems

what brand adapter and driver date and version?