Satellite A665 SLOW internet connection

Reply
Member
Posts: 2

Satellite A665 SLOW internet connection

Satellite A665-10013D

 

1 month old laptop and wondering Why am i getting a maximum of 290kbs speed only why my old A330 laptop is getting 1400 kbs. Even all connection are close and other laptops turn off.. im still getting a max of 290kbs. and i couldnt access to the internet using ethernet cables.. Why? 

Super Advisor
Posts: 1,052

Re: Satellite A665 SLOW internet connection

I don't know, but have you checked what firewall or other "security" software are installed on each machine?

Member
Posts: 2

Re: Satellite A665 SLOW internet connection

Thanks Brad but i've even tried closing all my firewall but its still the same. Even i've just formatted my laptop. the problem is still the same, and i still couldnt get connected with wired connection. i wonder why? would it be my network card problem? because i don think i got any virus because i've just formatted the laptop. 

Posts: 46,771
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Satellite A665 SLOW internet connection

 

Satellite A665-10013D (PSAW3L-07N00S)

 


i've just formatted the laptop. 

 

i .. couldnt get connected with wired connection


If the Ethernet connection doesn't work after you have restored the hard disk to its original out-of-the-box contents using Toshiba recovery media, then that's pretty serious.

 

What are you plugging in to?

-Jerry
Channel 9