|
|
|
01-23-2012 01:46 PM
After years of wireless connections wtih Satellite A105-S2716, both on-board G and usb netgear wireless N, I'm now unable to connect through ethernet port. FIOS in-home agent states there's no driver for wired network adapter found. I did do a clean re-install of XP SP3 about a year ago with original install discs from Toshiba.
Device Manager showed 2 Marvel Yukon ethernet adapters; '....08306....' was part of their name...I tried to update one of them; getting drivers from CNET indicating they matched my device number; tried to install; but marvell adapter device reported to be 'not working'; i had to rollback to previous driver. Then it showed as 'working' but didn't connect with ethernet FIOS.
the other marvel adapter i uninstalled, then couldn't find the device as it didn't appear in device manager; don't remember but it was the same number, but different name, than the other Marvell Yukon device.
So now I can only detect one Marvell device, have lost the other; and can't connect to ethernet.
Anyone know where I can get? i still have the original install disk with the OS but don't konw how to load drivers from it.
thanks!
pdoyle
01-23-2012 03:09 PM
It's here.
Marvell LAN Driver for Windows XP
All your drivers and utilities are here.
I did do a clean re-install of XP SP3 about a year ago with original install discs from Toshiba.
Toshiba did not supply install discs for Windows XP. You must have restored the hard disk to its original out-of-the-box contents using the Toshiba recovery media.
If so, then all of the correct drivers and utilities should have been in place
01-23-2012 04:07 PM
thanks Jerry...
yes you are correct, it is simply a recovery disc.
I already downloaded that Marvell driver; opened it with 7zip; thought I updated the Marvell ethernet device with the inf. file from the zipfile; restarted, but device mgr reported it didn't work. so i rolled back to previous driver, which device mgr says works, but no ethernet connection.
I did a power reset of the fios router/modem, turning devices on one by one...i can still connect wirelessly, but laptop so slow i'm hoping to get more speed with ethernet connectivity.
i'm using ethernet from a netgear switch, which is connected to my Fios router/modem mrw4214 or the like...that shouldn't matter, right?
under network connections it shows up as Incoming; but 'no client connection'.
maybe driver is ok; fios in-home agent software scans and says there's no network adapter for ethernet connection; so maybe it's missing hardware???
thanks! pdoyle
01-24-2012 06:28 AM
If you indeed restored the hard disk to its original out-of-the-box contents using Toshiba recovery media, then I don't understand what this is about.
Everything should work at that point.
01-24-2012 08:27 AM
Jerry, more effort and i think it may be hardware?
FIOS in-home agent software in trying to establish an ethernet connection to the home network, failed and reported it cannot find the ethernet adapter ; and advised that the laptop be taken to a pc repair shop....i'm now guessing that's hardware, there's no mention of drivers or software in the failure notice. Again, my on-board wireless G adapter works fine, and i normally run a netgear wirless N usb adapter for better speed.
I also tried your gigabit drivers; now the Marvell adapters are both reported to be "working" by device manager.
but network connections shows "incoming connection" but "no client". i assume that's the ethernet cat5 cable connected to the port.
do i need to modify the toshiba modem at all?
i downloaded DriverMax program from cnet; updated 2 drivers but i cannot tell which of the 23 drivers that program shows, would pertain to the ethernet connection...so i updated 2, but no apparent difference.
i did notice one of the marvell adapters says 'wireless' so i assume i ignore that one.
I also tried new connection wizard; to set up tcpip connection; then tried client; didn't have the driver; then tried protocol; didn't find the driver. i'm desperate.
I also tried the ping tests...127.0.0.1 etc. from microsoft; all the tests worked, except one; i forget which one.
any ideas please?
thanks pdoyle ![]()
01-24-2012 08:54 AM
No ideas. If things on the laptop don't work after the restore, the software is not the problem.
01-28-2012 10:22 AM
This is that im searching.
Thanks you for very useful information!
|
Copyright © 2011 Privacy Policy | Terms of Use | Forum Terms of Service | Contact Us Feedback
|
|