No Wi-Fi connection on Satellite P755-S5375 - Wireless Router working

Reply
Member
Posts: 3
Accepted Solution

No Wi-Fi connection on Satellite P755-S5375 - Wireless Router working

[ Edited ]

I have a Satellite P755-S5375 laptop running Windows 7 64-bit.  While working away from home on another network, my wireless connection dropped, and I have not been able to connect since. Smiley Frustrated  The other computers in the house are able to connect wirelessly, so it is something with my laptop.  Troubleshooting the problem indicated that my wireless connection is turned off.  The wireless icon on the laptop is lit, however, and when I try to toggle the Fn key and F8, nothing happens.  For further troubleshooting, I want to run the Toshiba utility to find out if there is another problem, but it seems to have been deleted; and when I search for the Value Added Package for P755 the results I receive are multiple pages not having to do with wireless or the P755.  Additionally, the Intel My WiFi Technology app is missing.  Device drivers are working fine, and I don't know where else to look.

 

My questions are:  Why is the Fn+F8 wireless toggle switch not working?

                            Where can I find the Value Added Package for my laptop?

                            Where can I go to download the Intel My WiFi Technology app?

 

Any help is appreciated.  I need to be free of my ethernet cable.

 

Here is info I received from entering, "Recovery" into Start, and choosing View Status:

Source

Intel(R) PROSet/Wireless Event Log Service

 

Summary

Stopped working

 

Date

‎12/‎19/‎2012 12:02 PM

 

Status

Not reported

 

Description

Faulting Application Path:     C:\Program Files\Intel\WiFi\bin\EvtEng.exe

 

Problem signature

Problem Event Name:            APPCRASH

Application Name:     EvtEng.exe

Application Version:  14.1.1.7

Application Timestamp:        4de6951f

Fault Module Name:  KERNELBASE.dll

Fault Module Version:           6.1.7601.17965

Fault Module Timestamp:     506dcae6

Exception Code:         c06d007e

Exception Offset:       000000000000bccd

OS Version:    6.1.7601.2.1.0.768.3

Locale ID:       1033

Additional Information 1:      a452

Additional Information 2:      a452cc5f22fd7b8acc3a1a4738d6c60c

Additional Information 3:      28bc

Additional Information 4:      28bc2bf47bfed00f83750dc2cdead9df

 


Accepted Solutions
Posts: 47,997
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: No Wi-Fi connection on Satellite P755-S5375 - Wireless Router working

 

Satellite P755-S5375

 

Downloads here.

 

 

I don't have any trouble locating things at the Toshiba website above. This looks like the TVAP.

 

   Toshiba Value Added Package

 

The "Intel My WiFi Technology app" is installed by the Proset utility.

 

   Intel My WiFi Technology is no longer available as a separate download

 

   Intel Proset

 

Some have been able to turn on the wireless by executing this file.

 

   C:\Program Files\Toshiba\TBS\TBSWireless.exe

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 47,997
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: No Wi-Fi connection on Satellite P755-S5375 - Wireless Router working

 

Satellite P755-S5375

 

Downloads here.

 

 

I don't have any trouble locating things at the Toshiba website above. This looks like the TVAP.

 

   Toshiba Value Added Package

 

The "Intel My WiFi Technology app" is installed by the Proset utility.

 

   Intel My WiFi Technology is no longer available as a separate download

 

   Intel Proset

 

Some have been able to turn on the wireless by executing this file.

 

   C:\Program Files\Toshiba\TBS\TBSWireless.exe

-Jerry
Channel 9
Posts: 47,997
Topics: 85
Kudos: 9,136
Solutions: 3,233
Registered: ‎12-04-2008

Re: No Wi-Fi connection on Satellite P755-S5375 - Wireless Router working


Jerry, thanks so much for your help.  I installed Intel Pro-Set and I'm back in business wirelessly! 

 Happy to help.

-Jerry
Channel 9