How can I enable Hosted network supported on my WiFi card?

Reply
Member
Posts: 1

How can I enable Hosted network supported on my WiFi card?

I have a laptop and I want to creat a virtual access point to use my laptop's Internet on my cellphone but I get this error:

"The hosted network couldn't be started.
The group or resource is not in the correct state to perform the requested opera
tion."

 

I tried to do it by command prompt but I couldn't start hosted network support!! the driver is updated!

What should I do?

 

my adapter information:

 Intel(R) PRO/Wireless 3945ABG

version: 13.4.0.139

Hosted network supported : No

 

 

C:\Windows\system32>netsh wlan show drivers

Interface name: Wireless Network Connection

Driver : Intel(R) PRO/Wireless 3945ABG Network Connection

Vendor : Intel Corporation
Provider : Intel
Date : 10/7/2010
Version : 13.4.0.139
INF file : C:\Windows\INF\oem43.inf
Files : 3 total
C:\Windows\system32\DRIVERS\NETwLv32.sys
C:\Windows\system32\NETwLc32.dll
C:\Windows\system32\NETwLr32.dll
Type : Native Wi-Fi Driver
Radio types supported : 802.11a 802.11b 802.11g
FIPS 140-2 mode supported : Yes
Hosted network supported : No
Authentication and cipher supported in infrastructure mode:
Open None
Open WEP-40bit
Open WEP-104bit
Open WEP
Shared WEP-40bit
Shared WEP-104bit
Shared WEP
WPA-Enterprise TKIP
WPA-Enterprise CCMP
WPA-Personal TKIP
WPA-Personal CCMP
WPA2-Enterprise TKIP
WPA2-Enterprise CCMP
WPA2-Personal TKIP
WPA2-Personal CCMP
Open Vendor defined
Authentication and cipher supported in ad-hoc mode:
Open None
Open WEP-40bit
Open WEP-104bit
Open WEP
Shared WEP-40bit
Shared WEP-104bit
Shared WEP
WPA2-Personal CCMP

 

C:\Windows\system32>netsh wlan show hostednetwork

Hosted network settings
-----------------------
Mode : Allowed
SSID name : "VirtualRouter"
Max number of clients : 100
Authentication : WPA2-Personal
Cipher : CCMP

Hosted network status
---------------------
Status : Not available


C:\Windows\system32>netsh wlan start hostednetwork
The hosted network couldn't be started.
The group or resource is not in the correct state to perform the requested opera
tion.

Posts: 47,926
Topics: 85
Kudos: 9,130
Solutions: 3,230
Registered: ‎12-04-2008

Re: How can I enable Hosted network supported on my WiFi card?

1. Which laptop? See the label on the bottom.

 

2. Which Windows and service-pack level?

 

3. Open Device Manager (devmgmt.msc) and expand Network adapters. Do you see Virtual WiFi Adapter?

-Jerry
Channel 9
Member
Posts: 2

Re: How can I enable Hosted network supported on my WiFi card?

Hey dude,

Sorry about this.

Intel had already declared that hostednetwork or wireless access point mode is not support in intel 3945ABG Wireless

Network Cards.

Member
Posts: 2

Re: How can I enable Hosted network supported on my WiFi card?

But its seems that we can make Wireless Access Point in Linux with the linux owned particular Drivers.

Using some programs like

1)airmon-ng

2)dhcp3

3)airbase-ng,etc

You can crawl google for some details.But this never ever acheived in Windows.