Ethernet controller driver

Reply
Member
Posts: 2

Ethernet controller driver

I can not connect to the internet with Ethernet cable. The wireless connection is working fine.

The device manager indicates that the driver for Ethernet controller is not installed.

On the Toshiba site for downloads I can not find the driver for the Ethernet controller.

I need to connect via Ethernet cable to install new router. Please help.

Computer: Toshiba Satellite L655-S5115 mod.PSK2CU-OFMO1U

 

Jan

Member
Posts: 2

Re: Ethernet controller driver

NOTE: Operating system on the computer is Widows 7      64 bit

Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: Ethernet controller driver

Your Drivers for your machine are here. The LAN driver is the first one on the list. Download it here.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit