Ethernet Adapter Missing???

Reply
Member
Posts: 3
Accepted Solution

Ethernet Adapter Missing???

Hi, I am a Toshiba user and for some reason there is no ethernet adapter (or driver) in my computer, therefore I cannot connect to the internet through ethernet cable. However, my wireless adapter is preinstalled in my laptop and it is working perfectly. Although, I need to use the ethernet cable for my workspace because I use this laptop very often. Any ideas on how I can obtain this driver? Adapter?

 

Specs:

C655-S5126 Toshiba Black Laptop

Windows 7 (pre-installed)


Accepted Solutions
Posts: 4,899
Topics: 57
Kudos: 1,685
Solutions: 386
Registered: ‎05-03-2009

Re: Ethernet Adapter Missing???

There is no C655-S5126 in Toshiba records.  I assume it's probably a C655D-S5126.  There is an Atheros LAN Driver for your machine.  I assume that's it but some confirmation from you would be helpful that the Atheros driver is the one you need--usually listed in Device Manager under Network Adapters.  See if the listing is still there. If there is no LAN adapter listed, give this one a try.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit

View solution in original post


All Replies
Posts: 4,899
Topics: 57
Kudos: 1,685
Solutions: 386
Registered: ‎05-03-2009

Re: Ethernet Adapter Missing???

There is no C655-S5126 in Toshiba records.  I assume it's probably a C655D-S5126.  There is an Atheros LAN Driver for your machine.  I assume that's it but some confirmation from you would be helpful that the Atheros driver is the one you need--usually listed in Device Manager under Network Adapters.  See if the listing is still there. If there is no LAN adapter listed, give this one a try.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 3

Re: Ethernet Adapter Missing???

Yes it is a C655D-S5126

 

I dont know where the device manager is. Can you kindly guide me to it? Thanks

Member
Posts: 3

Re: Ethernet Adapter Missing???

Thank you so much!!!!!

Posts: 4,899
Topics: 57
Kudos: 1,685
Solutions: 386
Registered: ‎05-03-2009

Re: Ethernet Adapter Missing???

I notice you marked my last post as Solving your problem but you still had a question about Device Manager.  Type Device in the Start/Search box, click on Device Manager, double click on Network Adapters and you should have a wireless adapter listed there and also a LAN adapter that may be called Family Controller which is the one that should be an Atheros. Right click it and it should tell you whether or not it is working properly.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 1

Re: Ethernet Adapter Missing???

Hey i have a Satelite C855D running windows 8(64bit) with the same problem, is the solution the same or is the process different?

Member
Posts: 3

Re: Ethernet Adapter Missing???

I hope this thread is still being monitored. I have the same issue with a brand new P855-S5102. The only adapter that shows up in "Network & Sharing" is WiFi. In Device Manager is WiFi plus "Microsoft Kernel Debug Network Adapter" whatever the he** that is. If I try to add a new device, the RJ45 can't be found.

HELP???

Thanx

Posts: 4,899
Topics: 57
Kudos: 1,685
Solutions: 386
Registered: ‎05-03-2009

Re: Ethernet Adapter Missing???

See my answer HERE.  Please do not double post.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit