Configfree stopped working- cannot install and reinstall Satellite L305-S5933

Reply
Member
Posts: 1

Configfree stopped working- cannot install and reinstall Satellite L305-S5933

[ Edited ]

"Configfree has stopped working" message appears on startup and whenever I click on the utility. Multiple attempts to install and reinstall do not fix this problem. Vista connects to my wireless system but the error message is annoying. I am stumped. This is my first Vista computer. Any suggestions. Error message:

Description:
  Stopped working

Problem signature:
  Problem Event Name:    APPCRASH
  Application Name:    cfmain.exe
  Application Version:    7.2.0.23
  Application Timestamp:    4861b6e6
  Fault Module Name:    KERNEL32.dll
  Fault Module Version:    6.0.6001.18215
  Fault Module Timestamp:    49953395
  Exception Code:    e0434f4d
  Exception Offset:    000442eb
  OS Version:    6.0.6001.2.1.0.768.3
  Locale ID:    1033

Thanks in advance,

Brog

Posts: 47,493
Topics: 83
Kudos: 9,023
Solutions: 3,198
Registered: ‎12-04-2008

Re: Configfree stopped working- cannot install and reinstall Satellite L305-S5933

 

Satellite L305-S5933 

 

You might try uninstalling the utility (Control Panel's Programs and Features) and rebooting before reinstalling.

 

   Config Free (32/64bit)

-Jerry
Channel 9