Cannot access internet through unsecured wireless networks

Reply
Member
Posts: 7

Cannot access internet through unsecured wireless networks

I recently bought a Toshiba Satellite L305D-S5930 with Windows Vista Home Premium. It has an Atheros AR5007EG Wireless Network Adapter. I have absolutly no problem connecting to my secured home wireless network. I do, however have a problem connecting to unsecured wireless networks. At first I was able to connect to unsecured wireless networks near my home, a neighbor I assume. At work I was able to connect to the unsecured wireless networks but with local/limited activity. I could not get internet access. Now even at home I can only get local access to unsecured wireless networks. I have spent hours searching the web looking to correct this problem and I have been unable to find a solution. My drivers are up to date. Please help before I pull all my hair out. Thanks!
Posts: 47,516
Topics: 84
Kudos: 9,032
Solutions: 3,200
Registered: ‎12-04-2008

Re: Cannot access internet through unsecured wireless networks

Satellite L305D-S5930 

I could not get internet access.

 

even at home I can only get local access


What does this mean exactly?

 

That your browser does not see web pages? What happens instead?

 

That you cannot send or receive email? What happens instead?

 

 

What happens when you're plugged into a router or modem?

 

  

 

  

-Jerry
Channel 9
Occasional Advisor
Posts: 1,169

Re: Cannot access internet through unsecured wireless networks

Is the unsecured network your own network?  Just because it is unsecured doesn't mean it is not protected.  And not all networks lead to the internet.
This signature left intentionally blank.
Member
Posts: 7

Re: Cannot access internet through unsecured wireless networks

So at home I can log onto my secured wireless network and access the internet. I was also able to log onto an unsecured network that I am assuming was a neighbors and could access the internet. In downtown Houston, where I work there are several hotspots and I was never able to log onto the network with local access only. Meaning I could not access the internet. I kept trying and tried the suggested windows automatic repairs but still nothing. Now all of a suden I can't even log onto the unsecured network in my apartments that I was able to log on to before. So in summary Access to the internet at home on my secured wireless network or a lan cable no problem. Access to the internet on an unsecured wireless network not happening.
Member
Posts: 7

Re: Cannot access internet through unsecured wireless networks

First off, thanks for the replies and any help you'll can give. At first when I try to log on to an unsecured network it would allow me to log on to the network but it would not give me internet access. When I viewed the network and sharing center it would show a connection to the network but then a red x on the connection fron the network to the internet. I have no problems when pluging in a lan cable or when connecting to my home secured wireless network. Also even though it shows me connected to a network I have never been able to find any other computers or printers on that network. There was also an unsecured network in my apartments I was able to log onto and view the internet. Now all of a sudden that does not work either. Basicly, my secured network allows me to access the internet fine all other unsecured networks will not. Maybe not all of the networks I have tried to log onto had access to the internet but I know some of them did.
Frequent Advisor
Posts: 891

Re: Cannot access internet through unsecured wireless networks

There was also an unsecured network in my apartments I was able to log onto and view the internet.

 

Perhaps the owner of the network has placed security on it since your last visit?

 

What happens when you remove security from your home network?

Posts: 47,516
Topics: 84
Kudos: 9,032
Solutions: 3,200
Registered: ‎12-04-2008

Re: Cannot access internet through unsecured wireless networks


 Access to the internet..

It's still not clear to me what you mean by this.

 

I assume a browser cannot surf the web. What is the message from IE7?

 

What about POP3 email access?

 

What about pinging?

 

   ping 209.85.171.100

 

   ping google.com

 

   ping localhost

 

When you cannot access the internet use this at the command prompt (cmd.exe) and paste the results in your reply

 

   ipconfig /all

-Jerry
Channel 9
Member
Posts: 7

Re: Cannot access internet through unsecured wireless networks

Jerry,

Here is the information you requested. Internet explorer gives me the following message:


Internet Explorer cannot display the webpage
Most likely causes:
You are not connected to the Internet.
The website is encountering problems.
There might be a typing error in the address.

I am not sure what you mean by POP3 email access. Here are the pinging results:

Pinging 209.85.171.100 with 32 bytes of data:
Reply from 192.168.1.254: Destination net unreachable.
Reply from 192.168.1.254: Destination net unreachable.
Reply from 192.168.1.254: Destination net unreachable.
Reply from 192.168.1.254: Destination net unreachable.

Ping statistics for 209.85.171.100:
    Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),


C:\Users\Marcus>ping google.com

Pinging homeportal.gateway.2wire.net [192.168.1.254] with 32 bytes of data:
Reply from 192.168.1.254: bytes=32 time=2ms TTL=255
Reply from 192.168.1.254: bytes=32 time=5ms TTL=255
Reply from 192.168.1.254: bytes=32 time=1ms TTL=255
Reply from 192.168.1.254: bytes=32 time=198ms TTL=255

Ping statistics for 192.168.1.254:
    Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),
Approximate round trip times in milli-seconds:
    Minimum = 1ms, Maximum = 198ms, Average = 51ms


C:\Users\Marcus>ping localhost

Pinging Black_Beauty [::1] from ::1 with 32 byte
Reply from ::1: time<1ms
Reply from ::1: time<1ms
Reply from ::1: time<1ms
Reply from ::1: time<1ms

Ping statistics for ::1:
    Packets: Sent = 4, Received = 4, Lost = 0 (0
Approximate round trip times in milli-seconds:
    Minimum = 0ms, Maximum = 0ms, Average = 0ms


Here are the "ipconfig /all" results:

Windows IP Configuration

   Host Name . . . . . . . . . . . . : Black_Beauty
   Primary Dns Suffix  . . . . . . . :
   Node Type . . . . . . . . . . . . : Broadcast
   IP Routing Enabled. . . . . . . . : No
   WINS Proxy Enabled. . . . . . . . : No
   DNS Suffix Search List. . . . . . : gateway.2wire.net

Wireless LAN adapter Wireless Network Connection:

   Connection-specific DNS Suffix  . : gateway.2wire.net
   Description . . . . . . . . . . . : Atheros AR5007EG Wireless Network Adapter

   Physical Address. . . . . . . . . : 00-21-63-FC-96-69
   DHCP Enabled. . . . . . . . . . . : Yes
   Autoconfiguration Enabled . . . . : Yes
   IPv4 Address. . . . . . . . . . . : 192.168.1.112(Preferred)
   Subnet Mask . . . . . . . . . . . : 255.255.255.0
   Lease Obtained. . . . . . . . . . : Tuesday, March 24, 2009 6:59:30 AM
   Lease Expires . . . . . . . . . . : Wednesday, March 25, 2009 7:15:47 AM
   Default Gateway . . . . . . . . . : 192.168.1.254
   DHCP Server . . . . . . . . . . . : 192.168.1.254
   DNS Servers . . . . . . . . . . . : 192.168.1.254
   NetBIOS over Tcpip. . . . . . . . : Enabled

Ethernet adapter Local Area Connection:

   Media State . . . . . . . . . . . : Media disconnected
   Connection-specific DNS Suffix  . : hsd1.tx.comcast.net.
   Description . . . . . . . . . . . : Realtek RTL8102E/8103E Family PCI-E FE NI
C
   Physical Address. . . . . . . . . : 00-1E-33-97-49-05
   DHCP Enabled. . . . . . . . . . . : Yes
   Autoconfiguration Enabled . . . . : Yes

Tunnel adapter Local Area Connection* 6:

   Media State . . . . . . . . . . . : Media disconnected
   Connection-specific DNS Suffix  . :
   Description . . . . . . . . . . . : isatap.hsd1.tx.comcast.net.
   Physical Address. . . . . . . . . : 00-00-00-00-00-00-00-E0
   DHCP Enabled. . . . . . . . . . . : No
   Autoconfiguration Enabled . . . . : Yes

Tunnel adapter Local Area Connection* 7:

   Connection-specific DNS Suffix  . : gateway.2wire.net
   Description . . . . . . . . . . . : isatap.gateway.2wire.net
   Physical Address. . . . . . . . . : 00-00-00-00-00-00-00-E0
   DHCP Enabled. . . . . . . . . . . : No
   Autoconfiguration Enabled . . . . : Yes
   Link-local IPv6 Address . . . . . : fe80::5efe:192.168.1.112%14(Preferred)
   Default Gateway . . . . . . . . . :
   DNS Servers . . . . . . . . . . . : 192.168.1.254
   NetBIOS over Tcpip. . . . . . . . : Disabled

Tunnel adapter Local Area Connection* 12:

   Media State . . . . . . . . . . . : Media disconnected
   Connection-specific DNS Suffix  . :
   Description . . . . . . . . . . . : Teredo Tunneling Pseudo-Interface
   Physical Address. . . . . . . . . : 02-00-54-55-4E-01
   DHCP Enabled. . . . . . . . . . . : No
   Autoconfiguration Enabled . . . . : Yes


Thanks again for your help.
Posts: 47,516
Topics: 84
Kudos: 9,032
Solutions: 3,200
Registered: ‎12-04-2008

Re: Cannot access internet through unsecured wireless networks

Let's see what happens after resetting IE7.

 

   How to reset Internet Explorer settings

-Jerry
Channel 9
Member
Posts: 7

Re: Cannot access internet through unsecured wireless networks

Reset internet explorer still no luck. Then just to complicate things I unsecured my home network and was able to connect to it and the internet. So the problem seems to take place only when connecting to other unsecured networks besides my own. I am so frustrated. Tomorrow I plan on going to a starbucks or burger king which I believe have unsecured free wifi and seeing if I can connect to their networks and access the internet through them. I will let you know how it goes.

Posts: 47,516
Topics: 84
Kudos: 9,032
Solutions: 3,200
Registered: ‎12-04-2008

Re: Cannot access internet through unsecured wireless networks


I unsecured my home network and was able to connect to it and the internet.

So the problem may have solved itself??

-Jerry
Channel 9
Member
Posts: 7

Re: Cannot access internet through unsecured wireless networks

No. I still only get local access when logged on to any other unsecured network other than my own. I want to see what happens when I go to a wifi hotspot. I just haven't had a chance yet. Hopefully, today or tomorrow.
Posts: 47,516
Topics: 84
Kudos: 9,032
Solutions: 3,200
Registered: ‎12-04-2008

Re: Cannot access internet through unsecured wireless networks

Peculiar situation. Most everybody else has more trouble with secured networks.
-Jerry
Channel 9
Member
Posts: 1

Re: Cannot access internet through unsecured wireless networks

 

Actually I am facing the similar problem, my laptop has no problem to access internet through my home secure wireless network. But when I try to access through hotspot or unsecure wireless network, like at McDonald and Starbuck, where they didnt require any wep code, my laptop unable to access internet even I can connect to their wireless network. My friend has no problem to connect to the hotspot using acer notebook at the same time.

Posts: 47,516
Topics: 84
Kudos: 9,032
Solutions: 3,200
Registered: ‎12-04-2008

Re: Cannot access internet through unsecured wireless networks

What computer? What Windows?

 

 

What happens when you turn off security in your home router?

-Jerry
Channel 9
Member
Posts: 7

Re: Cannot access internet through unsecured wireless networks

I have to say it is nice to know I am not the only one having this problem. I have windows vista and I honestly believe that is the problem. Don't get me wrong I am not a Vista hater. I am actually starting to like it but this network/internet thing is driving me crazy. I have read elsewhere where people are haveing wireless problems with vista while a machine with xp sitting right next to them has no problems at all. Unfortunetly I still have not find a solution to my particular problem.
Posts: 47,516
Topics: 84
Kudos: 9,032
Solutions: 3,200
Registered: ‎12-04-2008

Re: Cannot access internet through unsecured wireless networks

This is only the second person I've run across. But I know how you feel.

-Jerry
Channel 9