what are the keyboard shortcuts for Satellite L40-18X

Reply
Occasional Contributor
Posts: 16

what are the keyboard shortcuts for Satellite L40-18X

what are the keyboard shortcuts for Satellite L40-18X . i am asking for controlling sound volume and controlling brightness of the screen from keyboard. the problem is i didn't find how to use keyboard shortcut.

Occasional Contributor
Posts: 39

Re: what are the keyboard shortcuts for Satellite L40-18X

Fn+F6 = to turn the Brightness down

Fn+F7 = to turn the Brightness up

 

*for sound, there is no combination keys to adjust it. You can only adjust it by either using the volume knob or the Volume mixer.

Signature left blank intentionally
Posts: 47,702
Topics: 85
Kudos: 9,090
Solutions: 3,214
Registered: ‎12-04-2008

Re: what are the keyboard shortcuts for Satellite L40-18X

 

Satellite L40-18X

 

User Manuals are here.

 

   userman-en-20070719163316.zip (19/07/07)

 

   userman-en-20071120165207.zip (20/11/07)

 

For Windows Vista:

 

   Keyboard shortcuts

-Jerry
Channel 9
Occasional Contributor
Posts: 16

Re: what are the keyboard shortcuts for Satellite L40-18X

thank u very much for your help . the user manual helped me well. but i read in the user manual that there are a lot of shortcuts using fn+button and the only shortcut which work with me is fn+f6,f7 which control brightness . so please help me to use the remaining shortcuts . note that i have windows 7 ultimate on it . and if there anyway to activate these shortcuts please tell me .

Posts: 47,702
Topics: 85
Kudos: 9,090
Solutions: 3,214
Registered: ‎12-04-2008

Re: what are the keyboard shortcuts for Satellite L40-18X


i read in the user manual that there are a lot of shortcuts using fn+button

 

i have windows 7..


If the utilities that Toshiba wrote for Windows Vista (go here) don't work, you'll need to wait for utilities written for Windows 7.

 

Don't hold your breath.

-Jerry
Channel 9
Occasional Contributor
Posts: 39

Re: what are the keyboard shortcuts for Satellite L40-18X

Fn+Esc = Sound Mute

Fn+F1 = Lock

Fn+F2 = Power save Mode

Fn+F3 = Suspend

Fn+F4 = Hibernate

Fn+F5 = Display

Fn+F6 = Brightness Down

Fn+F7 = Brightness Up

Fn+F8 = Wireless Hotkey Switching

Fn+F9 = Disbaling or Enabling Touchpad

Fn+F10 = Cursor control overlay on and off

Fn+F11 = Numeric overlay on and off

Fn+F12 = Scroll feature on and off

Fn+Spacebar = Switches screen or video mode

Fn+1 = Zoom out with Zooming utility

Fn+2 = Zoom In with Zooming utility

Fn+Enter = Numeric Keypad Enter Key

Signature left blank intentionally
Occasional Contributor
Posts: 16

Re: what are the keyboard shortcuts for Satellite L40-18X

thank u for your help. i tried the link u told me . i found a lot of drivers so what is the best driver to update my lap to the latest update . please tell me the accurate name of the driver because i don't know what to choose from all of this drivers .

Posts: 47,702
Topics: 85
Kudos: 9,090
Solutions: 3,214
Registered: ‎12-04-2008

Re: what are the keyboard shortcuts for Satellite L40-18X

Sorry, but I don't know what to tell you.

-Jerry
Channel 9
Occasional Contributor
Posts: 16

Re: what are the keyboard shortcuts for Satellite L40-18X

okay , what i mean is i need any driver for activating keyboard shortcuts on windows 7 even if those drivers were created for vista 32 bit or 64 bit . so i am asking for the name of the most suitable driver which may work on windows 7 . and if no driver activate keyboard shortcuts so how can i make a request for new utilities for windows 7.

Posts: 47,702
Topics: 85
Kudos: 9,090
Solutions: 3,214
Registered: ‎12-04-2008

Re: what are the keyboard shortcuts for Satellite L40-18X

You know as much as I do.

-Jerry
Channel 9