touchpad

Reply
Member
Posts: 1

touchpad

Hello!

    I bought a brand new Toshiba Satellite L755 a few days back.My touchpad worked the first time I put on my laptop....but when I fixed an external mouse my touchpad stopped working completely.......it does'nt when work even when i remove the mouse...I need help fast... Thankyou!

Posts: 4,922
Topics: 57
Kudos: 1,717
Solutions: 387
Registered: ‎05-03-2009

Re: touchpad

[ Edited ]

Go to Control Panel/Mouse/Device Settings/Make sure your TouchPad is selected in the window and that the box just below the window is unchecked that says "Disable lnternal pointing device when external USB pointing device is attached". Click Apply if changes were made and OK.

 

In case you aren't aware, pressing FN+F9 toggles the TouchPad on/off.  Some models also have a small physical on/off switch located in the bottom keyboard bezel just below the center of the space bar.

 

If you need to post back here, please give your COMPLETE model info as in my examples below so we can be sure what features your model has.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit