Windows 8 Toshiba C855 Mouse Touch Pad locks after login of windows.

Reply
Member
Posts: 2

Windows 8 Toshiba C855 Mouse Touch Pad locks after login of windows.

Windows 8 Toshiba C855 Mouse Touch Pad locks after login of windows. I have four users login for this laptop. Only one user has locked Mouse Pad. I have tried restarting several times, FN key and F9 key, but neither helps.

 

Member
Posts: 2

Re: Windows 8 Toshiba C855 Mouse Touch Pad locks after login of windows.

The only thing F9 key does is decrease volume and F10 key increase volume. I do see a mouse pad symbol on the left edge of my space bar, but does not seem to toggle touch pad lock on of off. Still not sure what to do.

 

Posts: 21,713
Topics: 70
Kudos: 825
Solutions: 482
Registered: ‎10-04-2011

Re: Windows 8 Toshiba C855 Mouse Touch Pad locks after login of windows.

Can you check the laptop's full model and part numbers from the label on the bottom? Don't include the serial number.

- Peter
Member
Posts: 1

Re: Windows 8 Toshiba C855 Mouse Touch Pad locks after login of windows.

if your keyboard is setup (default) for the F buttons to do things like sound up/down or screen darker/lighter and you dont have to hit the FN button at the bottom of the keyboard (by CTRL) then hit the F5 button. otherwise hit (hold) FN and F5 together. the icons on it mean touch pad unlock/lock