Touchpad won't work with wireless mouse

Reply
Member
Posts: 2

Touchpad won't work with wireless mouse

I connected a Microsoft wireless mouse to my laptop and it was working fine. When I turned the computer on today the touchpad won't work at all. I tried disabling the mouse, but it's still the only thing that will work. I'd like to just get rid of the mouse and only use the touchpad. Any suggestions on how to do that? It's a Satellite L775D-S7305 laptop. Thanks.
Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: Touchpad won't work with wireless mouse

Go to Start/Control Panel/Mouse/Device Settings/Uncheck the box that says "Disable internal pointing device when external device is connected". Then, if necessary, toggle FN+F9 to turn Touchpad on.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 2

Re: Touchpad won't work with wireless mouse

Thanks.  I tried both of those things.  The "disable" box wasn't checked and toggling FN + F9 didn't work either so I finally just gave up.  This morning when I turned my computer on to give it a try, the touchpad wouldn't work at first and then when I came back to turn the computer off the touchpad WAS working.  And I didn't have the mouse connected or even turned on.  So it seems to be happening randomly.  I guess I'll just wait and see what happens.

Posts: 4,848
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: Touchpad won't work with wireless mouse

[ Edited ]

It may well have been an anomaly that will not occur again. I certainly hope so.

 

Good Luck!

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit