03-08-2012 08:48 AM
Hi,
I have got a new Toshiba Portege R830 and the toggle button above the touch pad isn't working. Can someone tell me what driver or software i need to install?
I have tried the Synaptics driver which didnt change anything. I have the flash card utility from the value added package installed but that only enables the function keys.
Thanks
03-12-2012 09:13 AM
Can you give the full model number? "R830" is only partial. It should be on a label on the bottom.
03-12-2012 09:32 AM
Portege R830-104
03-13-2012 01:25 PM
I don't see that model in the database. This site only officially supports the US region, so if it's from another region, I won't have any information on it. If that's the case, you might want to contact Toshiba customer support in another region.
Reinstalling the touchpad driver and TVAP is exactly where I would have started.
Try using System Restore to restore a previous restore point from before this became an issue.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.