Need to know what the F-keys do

Reply
Occasional Contributor
Posts: 25

Need to know what the F-keys do

I have a problem with the shortcuts coming on at unexpected times. Apparently, this can be fixed by pressing the Fn key and the NumLk key at the same time. However the NumLk key is not marked with letters. I suspect it is one of the function keys (F1 to F12) at the top, but they only have symbols. I downloaded the Users Guide, but it is password protected. (?)

 

Can anyone tell me what the function keys symbols mean? I have an 1135-S155 running Windows XP Hm SP2.

Toshiba Satellite L655d-S5151
Linux Mint 17 64 bit MATE.
VMware Player 6 with XP Home Edition SP2
Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Need to know what the F-keys do

 

Satellite 1135-S155 

 


I downloaded the Users Guide, but it is password protected. (?)

Huh?

 

   Satellite® 1130/1135 Series User’s Guide

-Jerry
Channel 9