Media touchpad not working

Reply
Member
Posts: 1

Media touchpad not working

Hello, I have a toshiba labtop.  Satellite series p755-S5265.  About 2 weeks ago the media touch bar stopped working (the one with the volume controls, eco mode, wireless on/off, etc).  What should I do?

 

I'm guessing I should first try to uninstall/reinstall some driver, but I'm not exactly sure which one, how to go about that or where to download the new one from.  Thanks in advance...

Posts: 4,812
Topics: 56
Kudos: 1,536
Solutions: 370
Registered: ‎05-03-2009

Re: Media touchpad not working

[ Edited ]

Uninstall TVAP (Toshiba Value Added Package).  Restart.  Reinstall TVAP located here:

 

                                                       P755-S5265 TVAP

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 45,953
Topics: 81
Kudos: 8,252
Solutions: 3,088
Registered: ‎12-04-2008

Re: Media touchpad not working

 

Satellite P755-S5265

 

 

If the TVAP reinstall doesn't work, we've seen this help. With the battery and AC adapter removed, close the Power switch for 30 seconds.

Re-attach those, press the Power button to turn the computer on, and then immediately press the F2 key while the Toshiba logo is displayed. Press F9 to restore the BIOS default settings, press F10, and then select Yes (Exit Saving Changes). The computer will restart.

-Jerry
Channel 9