L55-A5284 touchpad not working

Reply
Member
Posts: 3

L55-A5284 touchpad not working

[ Edited ]

Good day. Upon booting up my new Sattelite L55-A5284, the touchpad wouldn't respond. The function activation buttons don't make a difference, and there is no entry for the touchpad in the Device Manager under "Mice and Other Controllers", even after refreshing the information, and after trying to scan for and add new hardware.

 

Should I try downloading the touchpad driver, or is there a hardware connection issue? Thanks!

Member
Posts: 2

Re: L55-A5284 touchpad not working

I had the same problem with 2 of them. The 2nd one worked for a short time after updating windows. Now it no longer shows up in Device Mananger, even after downloading the drivers.

Posts: 21,719
Topics: 70
Kudos: 849
Solutions: 483
Registered: ‎10-04-2011

Re: L55-A5284 touchpad not working

Agent_K, do you have the same model?

 

Ophelia, I'm not sure what the problem is. Was it always like this, or was it working?

- Peter
Member
Posts: 2

Re: L55-A5284 touchpad not working

Yes, same model.

Member
Posts: 3

Re: L55-A5284 touchpad not working

As I mentioned, this is a brand new computer. The touchpad never worked, and there is no listing for it in the Device Manager.

 

If I try to download/install the touchpad driver, will it make any difference? Thanks!

Posts: 21,719
Topics: 70
Kudos: 849
Solutions: 483
Registered: ‎10-04-2011

Re: L55-A5284 touchpad not working

You could try it, but if it's brand new and never worked, your best option is probably to exchange it.

- Peter
Member
Posts: 1

Re: L55-A5284 touchpad not working

Had the same issue.  I have owned Toshiba's since 2005 and never seen anything like this.  Right out of the box the display did not come up.  Did the unplug and press power button trick and finally got the display to work.  Then noticed that the mouse pad would not come on.  Took it back to the store and they order me a new one.  Last night went back to the store and the same issue.  Mouse pad will not work.  Plugged in a mouse to navigate through the set up process and then the machine got stuck on a black screen for over 30 minutes.  At this time, after 2 brand new machines that would not work, I told the manager that I wanted my money back.  It is a shame that Toshiba is putting these crappy machines out there.  Does anyone do QA on these machines?

Member
Posts: 3

Re: L55-A5284 touchpad not working

Yeah, I was surprised to find mine didn't have bluetooth either. So I bought a bluetooth adapter and am using a mouse and keyboard with the computer plugged into my TV.

 

Not having the touchpad means that I MUST have the mouse with me when I take the laptop out of the house, but that's easily managed. I didn't want to have to deal with the exchange process and transferring my files again.

 

I think that I'll be avoiding Toshibas whenever I get new computers or other devices. Thanks for mentioning your experiences with them!

Member
Posts: 1

Re: L55-A5284 touchpad not working

Not sure if you were able to resolve your issue as it's been a while since anyone posted on this board, but I just ran into the same issue. Thankfully I was able to quickly find a resolution to this issue. Looking at the touchpad I noticed there was a light at the upper left corner of the mouse pad that was lit that I haven't seen as of yet, so it seemed a bit odd and kind of told me I had pressed a wrong button, upon further observation I noticed there was an odd symbol on the f5 key. So pressing that button I noticed the light on the mouse pad went out and returned my mouse pointer back to my desktop where it belonged. 

 

There again, if you haven't resolved your issued, give this little trick a try. 

Btw, the symbols on the f5 key has two icons on that button, one has two smaller squares under a larger one, the other looks similiar but also has the cicle with the line going across it down the center.

 

Give this a try if you still have that issue. Hope it works and good luck. Smiley Very Happy

 

If you do decide to go to another computer company, do yourself a favor and stay away from Dell. Just a little word of advice from personal experiences.

Member
Posts: 4

Re: L55-A5284 touched not working

I also have a brand new L55-NIRVANA bought in the US and the touch pad only worked upto the first steps of the setup process and then suddenly stopped working. I tried to uninstall and reinstall last version of drivers and nothing. Under the View menu of the  Device Manager I have to check "Show hidden devices" so that the Touch Pad driver appears under "Mice and other pointing devices". It reads "Synaptics SMBus Touchpad" with an alert sign over the icon. In Properties it reads "This device is not present, is not working properly, or does not have all its drivers installed. (Code 24)" in the Device Status comment area.

 

I also tried by making a system recovery and by using FN keys which by the way they no longer work too. I am starting to get bad tempered about this. It seems that Touchpad issues are generalized across the forums. I still cannot believe a brand like Toshiba is having such problems. 

 

Would you provide any alternative solution please?

 

 

Toshiba Satellite L55-A5284NR / Part No: PSKLAU -00H015

Member
Posts: 4

Re: L55-A5284 touched not working

It should read  L55-A5284NR

Member
Posts: 1

Re: L55-A5284 touchpad not working

I have a brand new laptop and it happens often.  Save these directions to fix it.   Toshiba should really fix this.   This is the last Toshiba I will buy.  It's my third Toshiba.

 

L55-A5284 touchpad

Try the following:

  • See if the Touchpad works when you unplug a USB mouse.
    If it does:
  1. Press the Windows Key + R to bring up the Run dialog.
  2. Type main.cpl and press Enter to bring up the Mouse properties.
  3. Click the Device Settings tab.
  4. Uncheck the “Disable internal pointing device when external USB pointing device is attached” option.
  • Press Fn+F9
    • On a lot of Toshiba Satellite models, this key combination will enable and disable the touchpad.
  • See if there is a Touchpad lock button
    • Some models have a button located between the spacebar and Touchpad itself. This is used to turn the function on and off.
Member
Posts: 4

Re: L55-A5284 touchpad not working

Thank you for your response but the touchpad doesn´t work either with mouse plugged or unplugged.

 

Member
Posts: 1

Re: L55-A5284 touchpad not working

This helped, in that at least the touchpad is now working. However, the touchpad does not show up in the device manager (even with viewing hidden devices), and the light on the touch pad still shows it is enabled. I unplugged all of my USB mice, so that only the touchpad should show, but the device manager somehow thinks my external microsoft mouse is plugged in and working when it is not plugged in at all. 

 

Any advice? 

 

My original issue was that the touchpad would just intermittently stop working, and the light would come on the touch pad showing it was disabled. Pressing F5 or FN+F9 made no difference at all. Originally, the touchpad was showing up in the device manager and I changed the settings to go back to my previous driver rather than the updated driver, then on restart the touch pad stopped showing up on the device manager. 

 

I have a S55D - 5383 with Windows 8.1.  Not even a month old. 

Thanks, 

 

crd

Member
Posts: 3

Re: L55-A5284 touchpad not working

[ Edited ]

Also running a L55-A5284.

 

I'm pretty frustrated, and that's making synthesizing all of this information pretty difficult.

 

History:

  1. Upgraded to 8.1
  2. Let Toshiba's update do it's thing
  3. Noticed malfunctioning mute button (F11)
  4. Updated keyboard driver (tc50156300g)
  5. Installed/uninstalled another Synaptics device (mouse)
  6. Messed with touchpad settings to add the regular scrolling feature
  7. Touchpad stopped working.

Now I'm at a point where I have the keyboard working, but the multifinger gestures and the scrolling function of the touchpad no longer work

 

This is what I've tried:

  • Off/On sequence from other videos
  • uninstalling/reinstalling drivers for mouse (newest and second to newest).  This works for about 30 seconds.
  • tried to install older system driver (which was stopped by windows)
  • Cursing, crying

(btw, the touchpad is turned on)  Smiley Tongue

 

Computer has been running now for a good 24 hours since I unboxed it, but it seems like this isn't an isolated problem.

 

Can any of you L55-A5284 brothers and sisters give me a step-by-step on what worked for you?

 

Thanks,

Nick

 

Posts: 4,922
Topics: 57
Kudos: 1,717
Solutions: 387
Registered: ‎05-03-2009

Re: L55-A5284 touchpad not working

Did you upgrade to 8.1 following very carefully the Toshiba instructions for the upgrade found HERE?

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 3

Re: L55-A5284 touchpad not working

C.B.

I, unfortunately, did not have the foresight to do so.  Am I SOL, or is there a grand restart-everything button?

 

Nick

 

Posts: 4,922
Topics: 57
Kudos: 1,717
Solutions: 387
Registered: ‎05-03-2009

Re: L55-A5284 touchpad not working

Nick, lots of folks have had success under the same circumstances by just following the update instructions I gave you AS IF you had not done the upgrade yet, restart and then let Toshiba Service Station do its thing per instructions after the upgrade. It's certainly worth a try and better than starting all over again by reverting to Win 8.

C.B.

Toshiba Sat. C75D-B7260 Win 10 Home 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Member
Posts: 3

Re: L55-A5284 touchpad not working

I ended up redoing the whole thing from scratch, but I'm picky like that.

 

Thanks for sending me to the instructions though, everything is working perfectly!

Member
Posts: 4

Re: L55-A5284 touchpad not working

[ Edited ]

I have a L55-A5226 but I've had similar problems. I've only had it since September or October.

 

As a poster above noted, the first issue I had was the the mute shortcut button stopped working. This happened within the first couple of months. It wasn't a big deal. Just today, I had the issue with the touchpad going out. It worked and after coming out of sleep mode, it didn't. The device did not show up in the menu. I deleted the driver and reinstalled it, and after restarting the computer, the touchpad worked again for a few seconds. I restarted again, and it worked for several hours but now has stopped working again. This time, though, the touchpad does show up in the device manager and it indicates it is working (although of course it isn't). It is turned on, and it does not work whether or not I have a mouse plugged in. Pretty frustrating that things have stopped working on a computer that has been in use for about 8 months. Any suggestions?

 

Note: After another restart of my computer, the touchpad works again, but I shouldn't have to restart the computer every couple hours to make it work.

 

Unrelated, but anothe issued I had with this computer is the pin in the SD slot broke after using it for only a couple months, so I have to hold the card in to use it.