FN and F1 keys

Reply
Member
Posts: 1

FN and F1 keys

Hello,

 

I am using an S855D-S5120 with WIN8.  I have looked but can't find an answer to what im trying to do.  I want to get my F1, F2, F3, and so on keys back to normal.  What they are set to default do is change the brightness, volume and other things, but in order to use F1, F2, so on i have to hold the FN key and than press F1, F2, and so on.  If you can pleasebrak this down on how to fix this.  Thank you guys.

Posts: 47,503
Topics: 83
Kudos: 9,028
Solutions: 3,198
Registered: ‎12-04-2008

Re: FN and F1 keys

 

Satellite S855D-S5120

 

 

That's Toshiba's new default.

 

   Function key changes in Satellite 800 series

 

There is an option in the UEFI (BIOS) to reverse that situation. See the section System Settings on p. 119 of the User's Guide.

 

   Satellite/Satellite Pro C800/L800/S800 Series User’s Guide

 

In System Settings, look for a Keyboard tab, with choices like these.

 

   Special function mode (Hold Fn first to use standard F1-F12 functions.)

 

   Standard F1-F12 mode (Hold Fn first to use special functions.)

-Jerry
Channel 9