09-18-2012 07:05 AM
I was wondering if there is a way to keep the ease of access program from having a defalt of using the keyboard as a mouse everytime I boot up? Everytime this is enabled it makes it so I cannot use my numeric or data entry Muntil I go in to the ease of access-mouse then uncheck use key board for mouse functions. Can this be done or am I stuck? Thank you in advance/ Mike
Solved! Go to Solution.
09-18-2012 07:36 AM
Mike, are you closing the Ease of Access window by clicking Apply and OK after you Uncheck the "Turn on Mouse Keys" box?
C.B.
09-18-2012 08:23 AM
Each time I do it I hit the apply button...then I go back to the main ease of access page. Everytime I boot up its selected again!
09-18-2012 08:28 AM
Here is exactly what I do. I deslect the mouse keyboard help, hit apply the apply button blanks out then comes back, then I hit ok and that takes me back to the main menu for ease of access. I reboot it goes back to original state ( selected and no numeric pad )
09-18-2012 08:33 AM
Two other things you can try.
1. Type msconfig in Start/Search box and click on msconfig.exe. Click the Startup tab and see if you can find something there that you can uncheck so it won't start automatically.
2. Type Services in Start/Search box and click on Services. A very long list but look in there to see if there is a service that you can stop that might solve the problem.
C.B.
09-18-2012 09:08 AM
Thank you so much for your help I finally found the problem. There was nothing in msconfig to help. I back tracked and noticed a "more settings" link went there and deselected everything there and found a setting using the num lock key. You had only two options for the num lock key. The mouse option was on with num lock key activtated nd I changed it to off since the num lock is on by default when booting up. Changing that setting took care of my problem 3 months after I bought the laptop...lol
09-18-2012 09:54 AM
You're welcome, Mike. Just happy you found a solution and thank you for reporting it back to us so that it may help someone else in the future.
C.B.
09-18-2012 04:02 PM
So it's this one..
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.