A665-S6050- Space Bar does not alway "space" when pressed

Reply
Member
Posts: 1

A665-S6050- Space Bar does not alway "space" when pressed

I just purchased a new Satellite I3 - Model A665-S6050 and notice that when I am typing and hit the space bar it does not always enter a space. This is becoming extremely annoying. I needto go back and enter spaces between words.  Has anyone else noticedthis same problem?  Is there a fix for this,other than getting an external keyboard. 

Otherwise, I like the compter so far, but the issue with the keyboard keys is enough to make me return the laptop and exchange it for another one...maybe a Sony?  This ismy first Toshiba and I am disappointed with the keyboard responsiveness.

 

Any feed back wouldbe appreciated!

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

I just got the Satellite A665 i7 and the spacebar is doing the same thing!  I researched for several months before buying a laptop. I decided to try a Toshiba and I now regret it.  I paid 1000.00 for this laptop and I expect the keyboard to work. It is very cheaply made as well. The performanceis great,(notice that it did not space) but what good is that when the keyboard does not work?  In addition to that this thing makes a very annoying buzzing sound as well as the keys make a "springing" sound when typing, it's drives me crazy!  I did call the company, they said I could send it to them to be fixed. I've only had it about two weeks.  Not impressed with Toshiba at all.  Another annoying feature of this laptop is that Toshiba vertical bar that shows up to the side of the screen ALL THE TIME. That thing is SO ANNOYING!  Toshiba: Make a quality keyboard if you are going to charge that much for a laptop!

Member
Posts: 3

Re: A665-S6050- Space Bar does not alway "space" when pressed

I am having the exact same issue and mineis only 2 weeks old.  It appears that when my thumb hits the space bar on the edge towards me, it doesn't activate a space, but if it i**bleep** in the middle to top edge (away from me) then I get a space.  This is a problem because my normal typing position causes my thumb to hit the forward halfof the space bar.  Also, thedisk drive isextremely loud from very high vibration.  Never seen one with this much vibration and noise.  Other than these two things, I'm happy, but these are both serious in my opinion.

Member
Posts: 3

Re: A665-S6050- Space Bar does not alway "space" when pressed

Oh, mine is a model A665-6059.

Regular Contributor
Posts: 131

Re: A665-S6050- Space Bar does not alway "space" when pressed

I'm currently FIGHTING with Toshiba on this issue and have a case number.  Depot repair could not duplicate the issue and returned the laptop unrepaired.

 

I'd each one of you to open "Notepad".  You cannot use Micosoft Word or a webpage to check the space bar.  Word may auto-correct the missing spaces.

 

Open Notepad by typing notepad in the search box.

 

Press the keyboard on the bottom edge.  I'll bet you won't get a space at all.  Please verify and post your results.

 

I went to a display model and pushed there and it worked like a charm.  My laptop is the A665-s6057.

 

So, you can try the bottom edge, left edge, top edge, right edge and at least 3 spots on the top of the space bar. With my laptop, the right edge gave some failures, but the bottom edge was 100% failures.

 

CompUSA's website had reviews with the same issue.

 

I can't post images directly and it's too much effort to set one up.

 

 

 

s8v
Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

Same problem with a Portege i7. Its quite annoying when you are focusing in writing  a paper. it shouldnt be a major problem for Toshiba to fix it . Is ther any hope besides buying an external keyboard ?

Regular Contributor
Posts: 131

Re: A665-S6050- Space Bar does not alway "space" when pressed

Toshiba has finally duplicated the spacebar problem.  It took them 45 days to do it.  So, it's being replaced.

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

Same here. Just sent it back after three days of trying to live with it. Ironically, to your post, I had a brand new sony vaio which was the smoothest laptop I have ever used...except that the audio was worde than a tin can (isn't sony an audio company too?). If this fix on the space bar works then all is well, otherwise, the pursuit for a perfect laptop remains.

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

I-have-a-Satellite-L505-S59903-my-space-bar-isn't-working-at-all-which-is-the-reason-this-emai-has-dashes-between-each-word-any-advice?

Member
Posts: 2

Re: A665-S6050- Space Bar does not alway "space" when pressed

Ok.  So I bought my Satelite R945-P440 and from day 1 the spacebar only worked if you hit it towards the middle.  I had forgotten to register it so I thought I was screwed.  Today I finally got sick of not having a working space bar.  

 

So I experimented.  First I looked at a video how to take this type of key off.  You have to be careful because it is annoying to get back on and you can break your hinges.  Before I explain my fix let me explain the reason it works.

 

 

Let is say this is the space bar and the mechanism under it.

 

 ________________

 ______  ^ _______

 

You hit the space bar in the center and it easily hits the sensor in the middle.  This is because all the weight is

on the center of the key.   When you hit the sides of the keys ( and youll notice the further from the center the more it happens ) the center of the key does not depress all the way.  This is what it looks like.

 

_ _ _ - _ _ _

____^_____   so the middle of the key never touches the sensor.  The fix?  Scotch tape.  Here is what you do.

 

Slowly with a blade or something VERY narrow pry the front right and left side of the spacebar up until it releases

from the plastic hinge.  Be careful NOT to pull the spacebar off or youll have to reconnect all the hinges and metal

inside, which is easy but annoying.  Make sure all the hinges are still connected etc then begin.

 

Under the key youll see a little circle.  Take 5 layers of scotch tape stuck together in a tiny square and stick it

to the bottom of the key center in the circle.  Make sure the tape doesnt stick out of the sides of the key or 

anything.  Just make sure it is large enuf to cover the little rubbin sensor on the keyboard when it is replaced.

 

Then snap the key back in place.  It should snap in easily.  Don't force it or you can break it.  Just make sure the

hinges are lined up etc.

 

As soon as you snap it in place, the center of the key is now closer to the rubber sensor.  This makes the key

extremely sensitive if you hit it in the middle ( which is why you cant use too much tape or it spaces by itself! )

and now when you hit the end of the key, since the middle of the key is now closer, it works!  Smiley Happy

 

Hope this easy fix helps.  It took me about 5 minutes!

 

Member
Posts: 2

Re: A665-S6050- Space Bar does not alway "space" when pressed

Read my fix...works great.  Same issue

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

i  have same problem with toshiba portege z935 p300   space bar non responsive one inch in from both sides

 

solutions    with hot melt gun i extruden hot mel on the for ends of thr bar   now when ihit the pace bar too farout i immediatey sense it and readjust

 

pain in ass   ive always bought toshibas   this is last one   ihave some other issues with theportege

 

mainly i like it as it is fast and light    but its lacking overall

 

ps one otherbad  feature   itis warped     probably being so cheaply made to be light   so that it wont lay flat

 

robert

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

Thank you, thank you!  I have searched again and again how to correct this problem.  So far it's working much better.

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

[ Edited ]

The Tape fix works! Super easy and fast. I took a little time to make sure I understood the parts and pieces under a spavebar (using youtube videos). I then did exactly as discribed and my spacebar nightmare is over!!

 

I am so happy. I was about to return this laptop. Not being able to type naturally is a deal breaker!!

 

COME ON TOSHIBA YOU CAN FIX THIS!!

 

 By the way I have the S55T-B5233

Member
Posts: 3

Re: A665-S6050- Space Bar does not alway "space" when pressed

I have the same problem!  This is crazy, I just bought it, loaded it all up with microsoft office and all my files and now I have to return it to Costco? I would like toshiba to pay me for my time.  Where do I send the bill?  I can't use a laptop that has a lagging or sticking spacebar.  Don't they quality test their products?? It seems to be with all of them. I have had to stop and respace six times just typing this one message and Im completely concentrating on makingsure I am spacing (which I should not have to do).  ERRRRR!

Here is anexample ofa linetyped and not fixed!!


smagy wrote:

I just purchased a new Satellite I3 - Model A665-S6050 and notice that when I am typing and hit the space bar it does not always enter a space. This is becoming extremely annoying. I needto go back and enter spaces between words.  Has anyone else noticedthis same problem?  Is there a fix for this,other than getting an external keyboard. 

Otherwise, I like the compter so far, but the issue with the keyboard keys is enough to make me return the laptop and exchange it for another one...maybe a Sony?  This ismy first Toshiba and I am disappointed with the keyboard responsiveness.

 

Any feed back wouldbe appreciated!


 

Regular Contributor
Posts: 131

Re: A665-S6050- Space Bar does not alway "space" when pressed

I bought a couple of top covers for the A665 series and one did have what seemed to eb an easy engineered fix.

The space key is lifted in two places  by a piece of foam insulation. 

 

The design of that area is really bad.  I have some pics somewhere.

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

I registered JUST to tell you thank you for this. I always knew it was something simple but couldn't fathom just HOW simple. My Toshiba L755 has been plaguing me with this annoyance forever now and I finally figured out exactly WHAT I was trying to look for. Many thanks again.

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

Thanks a lot, I bought an S55 brand new and I found out this problem with the keyboard, i sent it to techinal revission and it they didn't solve anything, I found this forum and your comment and It worked perfectly, the spacebar now works perfect in everyway.

 

Thanks a lot !!

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

This fix worked for me for the most part! I could not get over the way the key feld when pused in with the tape below it. I have figured out the cure for my laptop however.

 

I am using a Toshiba Satellite S55t-B with a backlit keyboard. When i took my spacebar completley off i notices that the edge closest to the track pad was raised considerably which casued the key to not press down evenly. There was a piece of light metal raised up from the keybaord tray so i used some tweezer and crimped it down. I was able to get it flush with everything else around it which allowed the key to be pressed in all the way and with even pressure.

 

I wish i would have taken photos but I wasn't sure it would work and after getting it put back together i didn't feel like taking it back apart. My problem was solved and I have yet to have the issue of an intermittent responce from the spacebar.

 

 

Member
Posts: 1

Re: A665-S6050- Space Bar does not alway "space" when pressed

I had the same problem with a brand new satellite c55-c  After reading the  posts I realized it was a mechanical problem  I thought sure it was  software.  Before dragging out my scotch tape I just pressed down firmly on the space bar.  there was a faint click and voila.