missing operating system

Reply
Member
Posts: 3

missing operating system

i have a toshiba DynaBook SS2000M which was given to me by a friend. if i ON it will give me a ''missing operating system''. can someone help me with this problem. thanks
Occasional Contributor
Posts: 43

Re: missing operating system

Does it have the hard drive?  If the hard drive is missing it will give this error.

 

If it does have the hard drive, it looks like the previous owner wiped the disk.

 

Is there a Windows sticker on the bottom of the laptop?  If so, which Windows version does it indicate?

 

You are going to need an install disk for Winows or the Toshiba recovery CD.

 

http://laptopforums.toshiba.com/t5/System-Recovery-and-Recovery/Recovery-media/td-p/9148