laptop powers on, no hdd light, does not load windows, dark screen - dead.

Reply
Member
Posts: 2

laptop powers on, no hdd light, does not load windows, dark screen - dead.

I have a Toshiba Satelite with intel processor, 1.5gig memory and a 250 G hdd...about 2.5 years old.

When I push the on button, the power light comes on, but that is it....does not access the hd, the hd inidcator light does not repsond at all when the on button is pressed....jsut sits there with a black screen.

I have searched this forum and googled and all but have not found this particular problem listed or a fix.

THe last week before this total failure, I had a number of times the computer would be fine and suddenly a blue screen would flash and the computer would reboot before I could read it. The last 2 times, if I moved the computer physically, picked it up from the floor or desk it would also go blue screen and reboot.

Any suggestions welcome.

Thanks,

Galen

Member
Posts: 2

Re: laptop powers on, no hdd light, does not load windows, dark screen - dead.

I got the same issues posted thread and no replys! Im about to just take out the H

 

Posts: 21,719
Topics: 70
Kudos: 849
Solutions: 483
Registered: ‎10-04-2011

Re: laptop powers on, no hdd light, does not load windows, dark screen - dead.

What model is it?

- Peter
Regular Advisor
Posts: 1,398

Re: laptop powers on, no hdd light, does not load windows, dark screen - dead.


galen wrote:

I have a Toshiba Satelite with intel processor, 1.5gig memory and a 250 G hdd...about 2.5 years old.

When I push the on button, the power light comes on, but that is it....does not access the hd, the hd inidcator light does not repsond at all when the on button is pressed....jsut sits there with a black screen.

I have searched this forum and googled and all but have not found this particular problem listed or a fix.

THe last week before this total failure, I had a number of times the computer would be fine and suddenly a blue screen would flash and the computer would reboot before I could read it. The last 2 times, if I moved the computer physically, picked it up from the floor or desk it would also go blue screen and reboot.

Any suggestions welcome.

Thanks,

Galen


As Peter indicated, please provide the full model number for your computer.  It is printed on the bottom.  Do not provide the serial number.

 

Does it matter whether the computer is plugged into the power adapter (and the adapter into a known working outlet) or just on battery power?

L305-S5955, T9300 Intel Core 2 Duo, 4GB RAM, 120GB SSD, Win 7 Ultimate 64-bit