Re: internet

Reply
Regular Member
Posts: 3

internet

unable to connect to internet with my wireless. even when i hook it up to the router(laptop satalite l 300 series model psl c8u-03q024) it says i am connected but no connection to internet it say i am off line.( say page cannot be displayed} my router is a tp-wr740n}tp-link .tried to reset the ip address to no prevail what to do ?email with tour answer.Smiley FrustratedRobot Frustrated

Highlighted
Posts: 48,195
Kudos: 9,189
Solutions: 3,261
Registered: ‎12-04-2008

Re: internet

 

Satellite L305D-S59222 (PSLC8U-03Q024)

 

Router TL-WR740N

 


even when i hook it up to the router


If both Ethernet and WiFi cannot see the Internet, there could be a problem in Windows' registry.

 

Try Microsoft's Fix it in both KB299357 and KB811259

-Jerry
Channel 9