cursor will not move

Reply
Member
Posts: 1

cursor will not move

Cursor will not move when Toshiba Satellite C650 is turned on - (laptop is plugged into the wall, not on battery) I've had this laptop for almost two years and never had any problems with it.

Super Advisor
Posts: 4,069

Re: cursor will not move

[ Edited ]

We need your full model name/number like Satellite C650-BT2N11. Also, if yours is not a USA model we need your model's part number like PSC08U-03G01E. Look on the Toshiba label on the bottom of your computer. We do NOT need your serial number.

 

But, first try pressing the Fn + F9 keys together, this allows you to enable and disable your touchpad, make sure it is enabled.

 

If this doesn't work, then let's try a system reset and see if this brings your touchpad back. Power off the laptop, unplug the AC from the unit, remove the battery, press and hold down the power button for 30 seconds, replace the battery and AC, power on, as soon as you see the Toshiba logo, press the 'F2' key to enter the BIOS Setup, in setup press 'F9' to load setup defaults, press 'F10' to save and exit, and then boot into Windows. Try the touchpad operation again, you may need to also press Fn+F9 to enable the touchpad.

 

Please let us know what happens. If this doesn't work, get back to us with your system info. Good luck.

 

Mike

 

Mike

Posts: 4,813
Topics: 56
Kudos: 1,537
Solutions: 370
Registered: ‎05-03-2009

Re: cursor will not move

Mike meant FN+F9 to toggle the TouchPad.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 7 HP SP1 64 Bit and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Super Advisor
Posts: 4,069

Re: cursor will not move


cbwilsha wrote: Mike meant FN+F9 to toggle the TouchPad. C.B.

What? It says Fn+F9 (after I edited it!)  Smiley Embarassed

 

Mike

Regular Advisor
Posts: 778

Re: cursor will not move

On the Satellite C600 series, in the Bios, under the Advanced->System Configuration settings is an Internal Pointing Device setting. Make sure it is Enabled.