Win 7 Blue Screen system_service_exception error (64-bit)

Reply
Member
Posts: 4

Win 7 Blue Screen system_service_exception error (64-bit)

I have gotten the Blue Screen listing system_service_exception twice in a row now. Usually occurs when running multiple internet tabs on Firefox, but no power-intensive programs except Word and/or Excel might be open. 

 

Error screen mentioned try to disable BIOS memory options such as caching or shadowing... before automatically rebooting... all Greek to me!!  Any help?  (When it DOES automatically reboot, it does so apparently fine.)

 

Machine is a Satellite L655-X5157 laptop running Windows 7 (64-bit).  Bought early in 2011 but only in use since August 2011. 

 

Attaching dump files after reading someone else's post.  I have no idea what these are or how to read them myself though.  Sigh... sorry, won't allow me to attach the files.  Will try to see if can log in to windows as admin and do so subsequently. 

Posts: 46,764
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Win 7 Blue Screen system_service_exception error (64-bit)

 

Satellite L655-S5157

 

Bug Check 0x3B: SYSTEM_SERVICE_EXCEPTION

 


Attaching dump files.. ... ..won't allow me to attach the files. 


The .dmp extension is not allowed in attachments. You can zip them up so they have the .zip extension. Or you can add the .txt extension to the end.

-Jerry
Channel 9
Highlighted
Member
Posts: 4

Win 7 Blue Screen system_service_exception error (64-bit)

Ok, folks, let's see if this worked... minidump files should now be attached.

 

Please help!  Not sure if this is a major issue or minor...

 

Also, would like to revise my typo previously:  the machine is a Satellite L655-S5157.  (not 'X')

 

Thanks

RP

Member
Posts: 4

Re: Win 7 Blue Screen system_service_exception error (64-bit)

Thank you!  Will try.  In my 2nd post I tried just copy n paste minidump files to My Docs folder and then attached from there.  Appeared to work, but not sure from your end? 

 

Will try again here from original location/folder using your method of adding .txt to the end.  Looks like I had to rename, removing .dmp and replacing with .txt, correct?  Does that damage the file?  Did this work? Thx.

Posts: 46,764
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Win 7 Blue Screen system_service_exception error (64-bit)

We didn't learn much from the .dmp files.

 

Try reinstalling your video driver.

 

   Intel Display Driver

 

==================================================

Dump File         : 011212-21200-01.dmp

Crash Time        : 1/14/2012 10:49:37 AM

Bug Check String  : SYSTEM_SERVICE_EXCEPTION

Bug Check Code    : 0x0000003b

Parameter 1       : 00000000`c0000005

Parameter 2       : fffff800`032bf528

Parameter 3       : fffff880`0a22b880

Parameter 4       : 00000000`00000000

Caused By Driver  : ntoskrnl.exe

Caused By Address : ntoskrnl.exe+7cc40

File Description  :

Product Name      :

Company           :

File Version      :

Processor         : x64

Computer Name     :

Full Path         : C:\Test\011212-21200-01.dmp

Processors Count  : 4

Major Version     : 15

Minor Version     : 7601

==================================================

 

==================================================

Dump File         : 011212-17347-01.dmp

Crash Time        : 1/14/2012 10:49:32 AM

Bug Check String  : SYSTEM_SERVICE_EXCEPTION

Bug Check Code    : 0x0000003b

Parameter 1       : 00000000`c0000005

Parameter 2       : fffff800`0326f528

Parameter 3       : fffff880`09d1c880

Parameter 4       : 00000000`00000000

Caused By Driver  : ntoskrnl.exe

Caused By Address : ntoskrnl.exe+7cc40

File Description  :

Product Name      :

Company           :

File Version      :

Processor         : x64

Computer Name     :

Full Path         : C:\Test\011212-17347-01.dmp

Processors Count  : 4

Major Version     : 15

Minor Version     : 7601

==================================================

-Jerry
Channel 9
Member
Posts: 4

Re: Win 7 Blue Screen system_service_exception error (64-bit)

Thank you. I re-installed Intel Display driver as recommended. All fine for a few days. Error recurred again today. I've deduced that it is happening during online banking sessions with Bank of America website. Could this narrow the source of the problem? (And I suspect I have not visited this site during the non-crash days in between, ie. since re-installing the driver, when all was running fine.) Running Firefox 9.0.1, which should be supported by the site. Thanks. RP
Posts: 46,764
Topics: 83
Kudos: 8,791
Solutions: 3,145
Registered: ‎12-04-2008

Re: Win 7 Blue Screen system_service_exception error (64-bit)


I've deduced that it is happening during online banking sessions with Bank of America website.

Switch to another browser for a  while and see what happens.

-Jerry
Channel 9