Unexpected Restart Happens But Restart Fails

Reply
Member
Posts: 1

Unexpected Restart Happens But Restart Fails

[ Edited ]

Please help!
I started having unexpected restarts a few weeks back. Now the problem is worse. This is now the second time where it reboots, but it doesn't complete the process. It reboots while it is rebooting! I got it to safe mode to check the settings for system failure, and it restarted again. All this is happening after I told Windows NOT to restart with a system failure. The only thing that has been able to get me back to normal for a few days is a System Restore initiated when I enter Safe Mode. Is this a Windows issue or could I have a hardware problem?
Here are my specs
Toshiba Satellite R25
2GB Ram
100GB Hard Drive
Windows XP Tablet
Thanks in advance.
I Brown

Posts: 48,208
Kudos: 9,191
Solutions: 3,262
Registered: ‎12-04-2008

Re: Unexpected Restart Happens But Restart Fails

Spontaneous restarts are often due to memory failures. Check it out.

 

   Windows Memory Diagnostic

-Jerry
Channel 9