Trouble installing SP3

Reply
Highlighted
Occasional Contributor
Posts: 48
Accepted Solution

Trouble installing SP3

I have got these messages that says the 2007 microsoft office suite SP3 is ready for installation but every time I try, the operation fails. I have gone to the microsoft site and tried installing from there but maybe I am not getting the message. Sp1 was already installed on this computer. Since then Sp2 has been added. Why does it keep telling me that the updates are ready for SP3. Do I really need them?I have just upgraded to IE9. Is that too high for this Toshiba Window Vista Basic Laptop L355 S7905?

Posts: 47,020
Topics: 83
Kudos: 8,912
Solutions: 3,164
Registered: ‎12-04-2008

Re: Trouble installing SP3

 

Satellite L355-S7905

 


the 2007 microsoft office suite SP3 is ready for installation but every time I try, the operation fails


Please attach a picture of the failure message.

 

In the meantime, run the Microsoft Fix it here.

 

   Fix the problem with Microsoft Windows Update that is not working 

 


Is that too high for this Toshiba Window Vista Basic Laptop..?


We have Office 2007 SP3 and IE9 installed on a 32-bit Vista machine. In fact, the Vista computer I'm making this message with has Office 2010. 

-Jerry
Channel 9

View solution in original post


All Replies
Posts: 47,020
Topics: 83
Kudos: 8,912
Solutions: 3,164
Registered: ‎12-04-2008

Re: Trouble installing SP3

 

Satellite L355-S7905

 


the 2007 microsoft office suite SP3 is ready for installation but every time I try, the operation fails


Please attach a picture of the failure message.

 

In the meantime, run the Microsoft Fix it here.

 

   Fix the problem with Microsoft Windows Update that is not working 

 


Is that too high for this Toshiba Window Vista Basic Laptop..?


We have Office 2007 SP3 and IE9 installed on a 32-bit Vista machine. In fact, the Vista computer I'm making this message with has Office 2010. 

-Jerry
Channel 9