Toshiba Satellite S50-A Wont Boot Power LED Lit

Reply
Member
Posts: 2
Accepted Solution

Toshiba Satellite S50-A Wont Boot Power LED Lit

Alright i just got my girlfirend a toshiba satellite S50-A. It worked all fine and dandy untill tonight after trying to turn it on she complained that it wouldn't.

On further observation I discovered that the power LED is turned on, which leads me to beleive the computer is powered on. But it is completely unresponsive. I have tried connecting a charger and the"I am now charging" LED WILL NOT light up.

I would like to attempt to pull the battery out but this model has a built in battery so in order to do so i would have to dissassemble it. Which normally wouldn't be a problem for me but since the LED for power is turned on I dont want to remove any hardware from the device at the risk of destroying anything.

It is BRAND new. Just got shipped to us last week,

 

 

 Product CodeProduct DescriptionQuantityTotal 
CONFIGURATIONCustom built computer1$599.99
BASE0253Satellite S50 customized1 
APP0041Office 365 30 day trial1 
APP10014Norton Internet Security 2013 30 day trial only1 
BAT00324 cell lithium-ion Battery1 
CAM0015Integrated HD webcam and microphone1 
COLOR0070Ice Silver in Brushed Aluminium1 
CPU0410Intel Core i3-3227U dual core processor1 
GFX0091Nvidia GT 740M 2GB dedicated graphics with Optimus1 
HDD0087500GB 5400RPM SATA hard drive1 
KEY0023Raised tile keyboard1 
LAN000210/100/1000 Gigabit Ethernet LAN1 
LCD009615.6" 1366X768 TruBrite LED backlit LCD1 
MEM01116GB (4GB+2GB) 1600MHz DDR3 memory1 
ODD0004DVD Supermulti drive +/- double layer1 
OS0127Windows 8 64 bit1 
PCB0098Motherboard type 21 
PEN0007No touch screen1 
SPKR0009harman/kardon stereo speakers1 
WARR00141 year standard warranty1 
WLAN0006Wireless b/g/n Wi-Fi

1

Above are the available specs from my order confirmation email. 

-Zach


Accepted Solutions
Member
Posts: 2

Re: Toshiba Satellite S50-A Wont Boot Power LED Lit

Fixed the problem my self. Turns out the back on this model actually comes off so it is REALLY easy to get to the motherboard, onboard battery, ram ect. 

 

Fix Solution:
Disconnect Internal Battery for 30 seconds

View solution in original post


All Replies
Member
Posts: 2

Re: Toshiba Satellite S50-A Wont Boot Power LED Lit

Fixed the problem my self. Turns out the back on this model actually comes off so it is REALLY easy to get to the motherboard, onboard battery, ram ect. 

 

Fix Solution:
Disconnect Internal Battery for 30 seconds

Posts: 2,923
Topics: 35
Kudos: 2,071
Solutions: 161
Registered: ‎07-26-2013

Re: Toshiba Satellite S50-A Wont Boot Power LED Lit

Could you please post some pictures of how to take the back off and what the insides and battery looks like, also how you remove the battery. Others like me are very curious about the new built-in battery and how to get to it and change or remove it, many questions have been posted on internet about this and i have not seen any good answers.

S70-ABT2N22 Windows 7 & 8.1Pro, C55-A5180 Windows 8.1 & W 10, Radius 12 Windows 10 ****Click on White “Kudos” STAR to say thanks!****
Member
Posts: 1

Re: Toshiba Satellite S50-A Wont Boot Power LED Lit

A similar problem with mine. Will not boot but mine has two LEDs lit. The "I'm on" and "plugged in and charging" is lit regardless of whether or not it is plugged in. It is less than a month old and they are making me pay to ship it to a repair center. Not happy.
Frequent Advisor
Posts: 2,331

Re: Toshiba Satellite S50-A Wont Boot Power LED Lit

Hi! Have you tried to disconnect the battery like the OP suggested??

A similar problem with mine. Will not boot but mine has two LEDs lit. The "I'm on" and "plugged in and charging" is lit regardless of whether or not it is plugged in. It is less than a month old and they are making me pay to ship it to a repair center. Not happy. 

 

I Love my Satellite L775D-S7222 Laptop. Some days you're the windshield, Some days you're the bug. The Computer world is crazy. If you have answers to computer problems, pass them forward.