Toshiba Satellite L775 Black Screen During Boot Up

Reply
Member
Posts: 1

Toshiba Satellite L775 Black Screen During Boot Up

I have a Toshiba Satellite L775 and I am having trouble with a black screen during boot up. I start the computer and it goes through to the windows starting screen then it goes to a black screen with arrow cursor. I can't get any response from the keyboard or anything. I didn't get any recovery discs with my computer so I don't know what to do. Any help is much appreciated!!!

 

Posts: 47,014
Topics: 83
Kudos: 8,912
Solutions: 3,164
Registered: ‎12-04-2008

Re: Toshiba Satellite L775 Black Screen During Boot Up


..it goes through to the windows starting screen

See if you can reach the Windows Recovery Environment using F8 and Repair Your Computer.

 

   What are the system recovery options in Windows 7?

 

Which Satellite L775? See the label on the bottom.

-Jerry
Channel 9