TosIPCSrv.exe stopped workING and was closed

Reply
Member
Posts: 2

TosIPCSrv.exe stopped workING and was closed

I have a Satellite A215-S5837 and everytime I boot up I get TosIPCSrv.exe stopped working and was closed.  No options on how to fix and my computer runs very slow.  I also can not get Vista SP2 to load and wondered if this TosIPCSrv.exe stopped working and was closed has anything to do with that.

Thanks,

Jeff

Posts: 47,042
Topics: 83
Kudos: 8,927
Solutions: 3,168
Registered: ‎12-04-2008

Re: TosIPCSrv.exe stopped workING and was closed

 

Satellite A215-S5837

 


TosIPCSrv.exe stopped working and was closed.


See if the fix here works for you, Jeff.

 

   TosIPCSrv.exe stopped working correctly (vista)

 

 


I also can not get Vista SP2 to load..


Meaning exactly what?

 

It doesn't appear at Windows Update?

 

It results in an error during installation?

 

Or what? Give the details.

-Jerry
Channel 9
Member
Posts: 2

Re: TosIPCSrv.exe stopped workING and was closed

Thanks Jerry, but that didn't work.  Until I can get the TosIPCSrv.exe stopped working and was closed resolved I am not going to try and install anything else.

Any other suggestions would be great.

Thanks,

Jeff

Posts: 47,042
Topics: 83
Kudos: 8,927
Solutions: 3,168
Registered: ‎12-04-2008

Re: TosIPCSrv.exe stopped workING and was closed

It should be easy to shut the message off.

 

Open the System Configuration utility (msconfig.exe) and uncheck the corresponding item on its Startup tab. 

-Jerry
Channel 9