Tecra laptop w/ external harddrive .. freezing on start up.. help

Reply
Member
Posts: 1

Tecra laptop w/ external harddrive .. freezing on start up.. help

[ Edited ]

I have a Toshiba Tecra laptop, I am using it with a Western Digital 500 gig external harddrive connected thru USB 2 connection.

 

The laptop freezes when I turn it on If I leave the external harddrive pluged to the USB port.  Can anyone help me in fixing this.  

Frequent Advisor
Posts: 2,022

Re: Tecra laptop w/ external harddrive .. freezing on start up.. help

it sounds like it is trying to boot to the external hdd and cant. this happens with alot of usb flash drives also.

-civicman4-
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Post all info about your laptop and version of windows. We are working on it but still do not have the powers to read your mind.